This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:c6678 uart fifo中断接收问题



器件:c6678 EVM板调试uart,采用

配置:fifo中断方式接收,配置成1byte trigger lever,fifo

现象:在单步模式下调试,uart edma中断服务函数中设置断点 , (1)通过上位机一次性发送5个bytes,查看到接收数组里收到这5个字节,但是后续填充了3个字节的随机值; (2)通过上位机一次性发送10个bytes,查看到接收数组里只收到了8个字节,丢了2个字节

上述问题是,不论接收数据有多少,fifo总是填充8个字节,我不清楚问题出在哪里?

请大师们指教!

  • http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/60482.aspx

  • 您好!

    我用的是6678的开发板,

    我的实验目的:计算机(PC机)给DSP开发板提供一个指令下发的当前时间(如:2015年1月28日10时05分26秒),这个时间作为DSP的数据处理的基准时间,然后DSP能够按照这个基准时间自己进行日期更新(类似于TMS320vc5509A中的RTC实时时钟模块),dsp处理完数据并将该数据上传至PC机,同时将DSP处理完的日期时间上传(如:处理完的日期是2015年1月28日12时05分26秒)

    我的问题:6678开发板能做这样的日历时间统计吗?谢谢