您好!刚接触C6657,使用TMDSEVM6657LS,CCS5.2.1.00018 ,在论坛里下载了STK_C6657_UART.7z软件例程,运行里面的Memory_Test工程,使用的PDK为pdk_C6657_1_1_1_4,编译后加载.out文件,加载到core_0报错,加载到core_1,程序能运行,但Memory_test结果错误,如下所示:
[C66xx_1] Memory Test with DMA fails at 0x10e05e20, Write 0x 0, Readback 0x 2104264000c0362
[C66xx_1] Memory Test with DMA fails at 0x10e05e28, Write 0x 0, Readback 0x 6000
[C66xx_1] Memory Test with DMA fails at 0x10e05e40, Write 0x 0, Readback 0x 2102264000c0362
[C66xx_1] Memory Test with DMA fails at 0x10e05e48, Write 0x 0, Readback 0x 6000
[C66xx_1] Memory Test with DMA fails at 0x10e05e60, Write 0x 0, Readback 0x1d738812028c1fd9
[C66xx_1] Memory Test with DMA fails at 0x10e05e68, Write 0x 0, Readback 0x 94736300100fd8
[C66xx_1] Memory Test with DMA fails at 0x10e05e70, Write 0x 0, Readback 0xd180a358c180a264
[C66xx_1] Memory Test with DMA fails at 0x10e05e78, Write 0x 0, Readback 0x 20c0fd8
[C66xx_1] Memory Test with DMA fails at 0x10e05e80, Write 0x 0, Readback 0x1ffb5c12008c1fd9
[C66xx_1] Memory Test with DMA fails at 0x10e05e88, Write 0x 0, Readback 0x 84736300100fd8
[C66xx_1] !!!Failed Memory Fill Test at 10 Units with pattern 0x 0 with EDMA CC0 TC1
[C66xx_1] Local L2 memory test at 189616739 cycle
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0x 0
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0xffffffffffffffff
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0xaaaaaaaaaaaaaaaa
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0x5555555555555555
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0xcccccccccccccccc
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0x3333333333333333
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0xf0f0f0f0f0f0f0f0
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0x f0f0f0f0f0f0f0f
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0xff00ff00ff00ff00
[C66xx_1] Passed Memory Fill Test from 0x 8226c0 to 0x 900000 with pattern 0x ff00ff00ff00ff
[C66xx_1] Passed Memory Address Test from 0x 8226c0 to 0x 900000
[C66xx_1] Passed Memory Bit Walking from 0x 8226c0 to 0x 900000
[C66xx_1] Passed Times: 7 Failed Times: 1
[C66xx_1] DDR3 memory test at 243235189100 cycle
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0x 0
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0xffffffffffffffff
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0xaaaaaaaaaaaaaaaa
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0x5555555555555555
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0xcccccccccccccccc
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0x3333333333333333
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0xf0f0f0f0f0f0f0f0
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0x f0f0f0f0f0f0f0f
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0xff00ff00ff00ff00
[C66xx_1] Passed Memory Fill Test from 0x80000000 to 0x80010000 with pattern 0x ff00ff00ff00ff
[C66xx_1] Passed Memory Address Test from 0x80000000 to 0x80010000
[C66xx_1] Passed Memory Bit Walking from 0x80000000 to 0x80010000
[C66xx_1] Passed Times: 18 Failed Times: 1
是例程有问题还是我操作的不对呢,谢谢答复!