This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747程序调试时遇到错误



tt.c为K均值算法,我想在C6747片中运行,可是当图片尺寸超过300*300时就会报错,说.far大小不够,.cmd文件也在附件中,请指点

C文件为:

#include <stdio.h>
#include <math.h>
#include "C6747.h"
#include <stdlib.h>      

///////////////////////////////////kmeans       
#define ROW 150     //** -输入数据每行数据个数 
#define COLUMN 150  //** - 输入数据每列数据个数 
#define K_clusters 2      //** - 所分数据的簇个数,它比实际值大1,比如:分5簇,该值应该设置为6 
#define num_km (ROW*COLUMN+1)      //** - 行列数据总个数,它为行列数据相乘再加1,比如:num_km=ROW*COLUMN+1; 
///////////////////////////////////kmeans

void kmeans(void);//Kmeans函数声明

///////////////////////////////////kmeans
 short int d_km[ROW][COLUMN]={1};
   //数据格式为灰度数据0-255之间的整数;如果为浮点数据,直接对浮点数据取整数才可以运算,因为灰度数据只能是整数
 int ind[num_km]={0};
 float old_cental[K_clusters],cental[K_clusters];   //经过kmeans算法处理之后的输出数据                 
 int d_km_out[ROW][COLUMN]={0},serial_km[num_km];//经过kmeans算法处理之后的输出数据
 #pragma DATA_SECTION(d_km,".ARRAY2");
 #pragma DATA_SECTION(ind,".ARRAY2");
 #pragma DATA_SECTION(serial_km,".ARRAY2");
 ///////////////////////////////////kmeans
void main(void)
{  int i,j;
   ///////////////////wzh
   /* output cluster label for each data point */  
  
       
   //////////////////wzh
 C6747_init();
    printf("DSP初始化结束\n");
    d_km[0][0]=1;
    for (i=1;i<COLUMN;i++)
       for(j=0;j<ROW;j++)
       {  d_km[0][0]=0;
       } 
       for(i=0;i<1000;i++)
         {
             kmeans();
          GPIO_OUT_DATA23=0xffff;//GPIO输出高电平
               kmeans();
            GPIO_OUT_DATA23=0x0000;//GPIO输出低电平
  
         }
    
}


/////////////////////////////////////////////////////functioon kmeans
void kmeans(void)
{
   int flag=0,temp;     
   int  i, j,k,km_temp=0;      
   float c[K_clusters]={0},m_a,m_h; 
   int h[257]={0};
   int aa[257]={0},hc[257]={0};
   float min_km=255,max_km=0,minmin=0;
   for (i=0;i<COLUMN;i++)
      for(j=0;j<ROW;j++)
    serial_km[i*ROW+j+1]=d_km[j][i];//对数据串行化处理
     
   for (i = 1; i < num_km; i++)
       {     
        if (serial_km[i] < min_km)
          {
           min_km = serial_km[i];
          }
       }//得到最小值数据
       minmin=min_km;//保存下最小值数据作为最后使用
   for (i = 1; i < num_km; i++)
   {  serial_km[i]=serial_km[i]-min_km+1;
      if (serial_km[i] > max_km)
          {
           max_km = serial_km[i];    
           }
 }
   max_km=max_km+1;
   //printf("max_km_%f \n",max_km);
      //% create image histogram
   km_temp=0;
    for (i = 1; i < num_km; i++)
 {  if(serial_km[i]>0)
          {
   h[serial_km[i]]=h[serial_km[i]]+1;
   km_temp++;
           }
 }//h(ima(i))=h(ima(i))+1;
 km_temp=1;
 //for (i = 1; i < 256; i++)
 //     {printf("%d ",ind[i]);}
 //     printf("\n ");
 for (i = 1; i < 257; i++)
 {  if(h[i]!=0)
    {    ind[km_temp++]=i;
    } 
 }//hl=km_temp;
 //hl=length(ind);
    //printf("km_temp_%d \n", km_temp);
    for (i = 1; i < K_clusters; i++)
 {cental[i]=i*max_km/(K_clusters);
 }// initiate centroids
  // printf("\n ");
 while(1)
    {for (i = 1; i < K_clusters; i++)
 {   old_cental[i]=cental[i];
 };//current classification  oldmu=mu;
     //ind,lengthind,h1
     for (i = 1; i < km_temp; i++)// for i=1:hl=km_temp
    { for(j = 1; j < K_clusters; j++)
         {c[j]=fabs(cental[j]-ind[i]);
        //  printf("c_%d ",c[j]);
       }                     //c=abs(ind(i)-mu);
      // printf("\n");
    min_km=255;//每次循环都初始化
   for (j = 1; j < K_clusters; j++)
    {if (c[j] < min_km)
   {
              min_km = c[j];
        temp=j;//temp=cc(1);
         }
    }
   // printf("min_%d ",min_km);
      hc[ind[i]]=temp;//hc[ind[i]]=temp;
  }//end for
   for(i = 1; i < K_clusters; i++)//  for i=1:k
 {  k=1;  
       for (j = 1; j < 257; j++) //全局搜索
    {   //printf("hccc_%d ",hc[j]);
     if(i==hc[j])
     {
     aa[k]=j;
     k++;
     }  
    }//a=find(hc==i); 
    m_a=0;
    m_h=0;
      for (j = 1; j < k; j++)
   {m_a=m_a+h[aa[j]];
   }
      //printf("m_a_%f ",m_a);
     // printf("k_%d ",k);
   for (j = 1; j < k; j++)
   {aa[j]=aa[j]*h[aa[j]];
       m_h=aa[j]+m_h;
   }
  // printf("m_h_%f\n ",m_h);
     cental[i]=m_h/m_a;
 } // mu(i)=sum(a.*h(a))/sum(h(a));
    flag=0;
    for(i = 1; i < K_clusters; i++)
       {if (cental[i]!=old_cental[i])
           {flag=flag+1;}
       }
    if (flag==0)
       {//printf("\nflag=%d\n",flag);
        break;}
    
 }//end while
   //% calculate mask   
   //printf("over");
   for(i = 0; i < ROW; i++)
   {
      for(j = 0; j < COLUMN; j++)
       {   for(k = 1; k < K_clusters; k++)
          {c[k]=(int)fabs(cental[k]-d_km[i][j]);
            } //c=abs(copy(i,j)-

        min_km=255;
           for (k = 1; k < K_clusters; k++)
           {if (c[k] < min_km)
             {
             min_km = c[k];
    km_temp=k;
             }  
           }//a=find(c==min(c));
          d_km_out[i][j]=km_temp;
         // printf("%d ", d_km_out[i][j]);
       }
     //  printf("\n ");
   }//% calculate mask end
   for (k = 1; k < K_clusters; k++)
   {cental[k]=cental[k]+minmin-1;
   };
   //mu=mu+mi-1;   % recover real range
   printf("over!");

}

CMD文件:

-l rts6700.lib
 -l dsp67x.lib


-stack           0x00001000      /* Stack Size */
-heap            0x00001000      /* Heap Size */

MEMORY
{
    VECS:        o = 0x80000000  l = 0x00000f00
    ARMRAM:      o = 0xFFFF0080  l = 0x00001f80
    DSPL2RAM:      o = 0x00800000  l = 0x00040000
    SHAREDRAM:   o = 0x80000f00  l = 0x0001ffff
    SDRAM1:       o = 0xC0000000  l = 0x00800000
    SDRAM2:      o = 0xC0800000  l = 0x03800000

}

SECTIONS
{   ".vectors"  >   VECS
    .bss        >   DSPL2RAM
    .cinit      >   DSPL2RAM
    .cio        >   DSPL2RAM
    .const      >   DSPL2RAM
    .stack      >   DSPL2RAM
    .sysmem     >   DSPL2RAM
    .text       >   SHAREDRAM
    .switch     >   DSPL2RAM
    .far        >   SHAREDRAM
    .ARRAY1     >   SDRAM1
    .ARRAY2     >   SDRAM2
}