This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NAND ubifs启动失败



之前在通过烧写EVM板上NAND能顺利运行的ubi.img,放到自己做的板子上启动到ubi就出现了错误,

自己的板子上用的NAND是Spansion的2Gb X8 TSOP Flash,只支持1bit ECC

怀疑是ECC存在问题,

sysboot配置是选择了ECC handled by NAND

在board_am335xevm.c中发现

static void evm_nand_init(int evm_id, int profile)
{
struct omap_nand_platform_data *pdata;
struct gpmc_devices_info gpmc_device[2] = {
{ NULL, 0 },
{ NULL, 0 },
};

setup_pin_mux(nand_pin_mux);
pdata = omap_nand_init(am335x_nand_partitions,
ARRAY_SIZE(am335x_nand_partitions), 0, 0,
&am335x_nand_timings);
if (!pdata)
return;
pdata->ecc_opt =OMAP_ECC_BCH8_CODE_HW;
pdata->elm_used = true;
gpmc_device[0].pdata = pdata;
gpmc_device[0].flag = GPMC_DEVICE_NAND;

omap_init_gpmc(gpmc_device, sizeof(gpmc_device));
omap_init_elm();
}

像我这种只支持1bit ECC的Flash应该用什么ecc_opt ?

请高手指导,谢谢!

PS: BSP版本为:linux-3.2.0-psp04.06.00.11