This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 I2C NAND BOOT



ALLEN 您好:

我在使用6657通过I2C做NAND BOOT,有以下问题:

1.官方例程要求BOOTMODE【11:10】设置为01,但是BOOTMODE【12:10】同时也是PLL的设置管脚,我们的板卡上面核输入时钟是100MHz,按照手册应该将bootmode[12:10]设置为011,因此与I2C  BOOT要求的EPROM地址不一样,地址从0x51变成了0x53,想请教您一下在这种情况下还可以通过0x51来boot么,如果不可以如何通过0x53boot

2.我们也可以将核时钟将为50M,因此地址也可以变为0x50,如果0x53不可以的话0x50是不是也可以,如何来改官方例程