This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6467 HD 1080P EVM 求助!!



本人手上有一块tms320dm6467 HD 1080P EVM板卡,按照以下步骤:

1,运行i2c_eeprom_writer.out,烧写ubl_dm646x_297.bin到I2C EEP

2,运行nand_flash_writer.out,烧写u-boot-1.2.0-dm6467.bin到nand

3,运行setmac.out烧写MAC地址

然后设置成I2C启动,但是,启动后在超级终端中显示如下:

Booting PSP Boot Loader

 

Starting NAND Copy

 

Booting Application @ 0x81080000

然后就停止了。这个问题困扰我好多天了,一直没能解决,求高人解答。

本人在CCS3.3下运行tests中的nandflash测试程序,flash是正常的。忘论坛中高人指点指点。