1 编译时先时出现很多dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: In function 'INIT_LIST_HEAD':
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:26:6: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:27:6: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: At top level:
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:39:17: warning: 'struct list_head' declared inside parameter list [enabled by default]
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: In function '__list_add':
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:41:6: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:42:5: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:43:5: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:44:6: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: At top level:
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:60:59: warning: 'struct list_head' declared inside parameter list [enabled by default]
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: In function 'list_add':
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:62:28: error: dereferencing pointer to incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:62:2: warning: passing argument 1 of '__list_add' from incompatible pointer type [enabled by default]
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:37:20: note: expected 'struct list_head *' but argument is of type 'struct list_head *'
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:62:2: warning: passing argument 2 of '__list_add' from incompatible pointer type [enabled by default]
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:37:20: note: expected 'struct list_head *' but argument is of type 'struct list_head *'
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: At top level:
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:74:64: warning: 'struct list_head' declared inside parameter list [enabled by default]
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h: In function 'list_add_tail':
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/list.h:76:22: error: dereferencing pointer to incomplete type
2 fatal error: asm/rwsem.h: No such file or directory
最后又出现
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/rwsem.h:29:19: error: field 'wait_list' has incomplete type
../../../ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include/linux/rwsem.h:41:23: fatal error: asm/rwsem.h: No such file or directory
然后我找了下确实没有asm/rwsem.h这个文件,搞了一天没搞懂。
这是我的pro的配置文件内容
TEMPLATE = app
CONFIG += console
CONFIG -= app_bundle
CONFIG -= qt
SOURCES += main.c \
unix.c \
timers_unix.c \
timer.c \
sync.c \
symbols.c \
states.c \
sdo.c \
pdo.c \
objacces.c \
nmtSlave.c \
nmtMaster.c \
lss.c \
lifegrd.c \
emcy.c \
dcf.c \
can_socket.c \
ObjDict.c
OTHER_FILES += \
canopen_canfestival.pro.user
HEADERS += \
timers_driver.h \
timerscfg.h \
timer.h \
sysdep.h \
sync.h \
states.h \
sdo.h \
pdo.h \
objdictdef.h \
objacces.h \
nmtSlave.h \
nmtMaster.h \
lss.h \
lifegrd.h \
emcy.h \
def.h \
dcf.h \
data.h \
canfestival.h \
can_driver.h \
can.h \
applicfg.h \
ObjDict.h \
config.h
target.path += /home/root
INSTALLS += target
INCLUDEPATH += /home/ti-sdk-am335x-evm-06.00.00.00/
INCLUDEPATH += /home/ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/include
INCLUDEPATH += /home/ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/arch/arm/include
INCLUDEPATH += /home/ti-sdk-am335x-evm-06.00.00.00/board-support/linux-3.2.0-psp04.06.00.11/arch/arm/include/generated
请大神来解答啊,急急!!!!
qt按照TI的hands on with qt文档上配置的,也source了,helloworld能编译通过,并能在beaglebone black板上运行