This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365死机问题

Other Parts Discussed in Thread: TPS65053

一共做了5套DM365电路板,各板都不同程度的出现了司机现象.

DM365死机可能出现在任何位置,如在内核解压过程,内核启动过程,程序运行过程都可能出现死机,在内核解压和启动过程中死机可能性较大.

5V安捷伦电源供电,电源芯片使用TPS65053RGE,5V电源入口端未使用去耦电容,TPS65053转换的1.2V,1.8V.3.3V电源都使用0.1uF与10uF电容去耦.

使用专用的复位芯片TCM811SERC进行各芯片上电复位.

DDR布线使用等长处理.

基本情况如上,如有还需要我提供的情况请告知,我会补充. 

麻烦技术人员分析一下可能出现死机的原因,谢谢.