This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 如何访问PCIe EP设备配置空间?



  你好,我在调试DM8168 PCIe 时,遇到一些问题,如下:

      1、DM8168作为RC时,如何访问PCIe EP的配置空间?我用的EP设备是FPGA PCIe IPcore。可以映射I/O空间和Mem空间。

      2、DM8168 上有一段地址空间:0x2000 0000 -0x2FFF FFFF 共256M,这个空间是具体用来做什么的?

      3、DM8168 有一个大小是4KB的Remote Device Config SpaceType 0 / Type 1 (4 KB),通过访问这个空间是不是可以访问 远端PCIe EP设备的配置空间?

  期待您的回答~   谢谢~