本人自行编写的二次加载(Pageload)程序在CCS3.3开发环境下通过连接仿真器可以将FLASH中的用户程序搬移到DSP的RAM中并能保证其正确运行。但是,当我将二次加载(Pageload)程序烧写到FLASH中,想利用C5509A内部固化的bootloader先完成二次加载(Pageload)程序的加载,然后再完成用户程序的加载时出问题了,程序加载后只能执行一部分,另外DSP与FLASH是通过EMIF进行连接的。不知道到底是什么问题,困扰很久了,希望有人可以指教,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.