This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x调试问题-VDDS电源对地短路



故障现象:AM335x芯片上电之后,芯片开始发烫,TPS65910A3的VDAC电源输出为1.44V(正常1.8V)。测得此时VDAC电源的输出电流为204mA(VDAC最大输出电流为150mA)。断电之后测量VDDS与DGND之间短路。断开VDAC电源与AM335x的连接,上电后AM335x不发热,用示波器观察VDAC的商店波形,没有发现尖峰。其他电源上电正常。

存在问题:原理图抄的Starter Kit-TMDSSK3358原理图,VDDS电源输入端没有放置10uF电容。

已做工作:检查过原理图绘制,检查过AM335x的原理图封装与PCB封装。

问题:(1)VDDS是否为上电过程中的重要电源,他的不正常对上电过程有什么影响?

            (2)VDDS上电短路的原因可能是什么,是因为电源输入端没有放置10uF电容,还是I/O连接错误导致电源短路?

            (3)在其他电源正常的情况下,VDDS连接1.8V之后,AM335x是否就可以通过UART0打印CCC....?

            (4)调试过程中还应注意哪些问题?

请高手不吝赐教,谢谢。