This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的工程师们你们好。
我现在使用的是深圳天漠的Devkit8500开发板,现在在移植他人在DM642的算法时,发现其用了dm642的CSL(chip support library)库里面的DAT_copy函数,该函数利用DM642的DMA进行源数据到目的数据的复制,现在我想在DM3730上使用这些函数,但是,查到一些资料说,TI不支持在codec engine上面使用csl库,请问是这样的么?并且我在CCS5.2以及DVSDK包里均没有发现CSL库的存在。如果我在codec engine工程中使用这一类的函数,我应该用哪一个库哪一个函数呢?、
谢谢。
hi
I am using devkit8500 and dvsdk_4_03 now.
I copide an example in codec-engine_2_26_02_11 for my development. And I need a function which can transmit data using DMA in DSP side, just like the DAT_copy function in CSL ( chip support library). which library and function can I use ?
Can I use the CSL on DM3730 ?
你好,我也再用devkit8500和dvsdk4-03,但我在编译dmai时提示有文件出错:
ake[2]: *** [obj/linux/omap3530/Capture.dm3730.o470MV] Error 1
make[2]: Leaving directory `/home/davinci/dm3730/dvsdk4_03/dmai_2_20_00_15/packages/ti/sdo/dmai'
make[1]: *** [all] Error 2
make[1]: Leaving directory `/home/davinci/dm3730/dvsdk4_03/dmai_2_20_00_15'
make: *** [dmai] Error 2
我按照路径去找,发现根本没有这些文件,请问你有遇到过这问题吗?