This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8168双流编码问题



各位好!

    我现在用使用dm8168进行双流编码测试,采用rdk的mcfw框架,link的配置如下图所示:

现在测试16路视频的捕获,16路D1编码及输出都正常,现在的问题是,添加16路cif后,有如下问题:

1.如果右边两个蓝色的merge不经过nsf直接连接,则经过编码后,16路D1编码正常,前8路cif有数据,但后8路cif没有数据

2右边两个蓝色merge间加入nsf link,经过编码后,16路d1编码正常,16路cif都有数据,但图像不正常,现象为图像宽度压缩到原来一半,左半边图像基本呈绿色和红色,右半边图像为灰色块。如图:

通过修改nsf link的创建参数,均不起作用,请专家或高手指点一下如何解决。