我用的JLINK调试器,cpu是Ti的AM3505,scriptfile是用的sample里面的AM3517.Scriptfile。JLink.exe可以正常识别如下图:
可是GDBserver无法识别A8内核,请问是什么原因。脚本文件已发附件。。。。有谁遇到过类似情况的?
JLinkARM.dll V4.84e (DLL compiled Apr 28 2014 20:59:12)
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: yes
Generate logfile: off
Verify download: off
Init regs on start: on
Silent mode: off
Single run mode: off
Target connection timeout: 5 sec.
------J-Link related settings------
J-Link Host interface: USB
J-Link script: Default.JLinkScript
J-Link settings file: none
------Target related settings------
Target device: AM3505
Target interface: JTAG
Target interface speed: 100kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link V9 compiled Apr 15 2014 19:08:28
Hardware: V9.00
S/N: 59047936
Feature(s): GDB, RDI, FlashDL, FlashBP, JFlash
Checking target voltage...
Target voltage: 3.30 V
Listening on TCP/IP port 2331
Connecting to target...WARNING: Identified core does not match configuration. (Found: None, Configured: Cortex-A8)
J-Link found 2 JTAG devices, Total IRLen = 10
JTAG ID: 0x0B6D602F (ARM7)
ERROR: Could not connect to target.
Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...
Shutting down...