This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询下关于 mcasp 使用时在49.152MHZ使用时,出现不稳定现象,如何解决?



在Dm6467 mcasp0上使用 rx0 接收IIS格式的音频信号,

采样频率为48KHZ,每个时隙采用32bit位宽,32个时隙进行接收时,发现音频通道虽然可以运行,但是在arm新运行程序时,总是发生RBUF来不及搬运出数据而导致的overrun,如果在系统稳定运行时运行音频接收程序,则不会出现overrun.

请问MCASP0可以设置在RHCLK及RCLK是否可以在49.152MHZ下正常使用? 因为没有使用smartreflex,也排除了电源供电不稳的原因,DDR,EDMA单独测试的速度均能满足要求,由于EDMA没有使用L2,而直接将目的地址指向了DDR2(297MHZ),arm应用程序访问DDR2会导致EDMA速度急速下降吗?