我在设计DM368与CMOS的接口时遇到问题,具体如下:
1. CMOS的VDD_IO电压是1.8V/2.8V,两个电压选择一个。而368的ISIF Power supply是1.8V。我的理解是CMOS的VDD_IO选择1.8V,然后就可以直接与368的ISIF连接了。我的理解是否正确呢?
2. 我在TI的官网上看到的368的参考原理框图(见下面图片)中在CMOS与368的ISIF之间加入了具有三态输出的电平转换收发器,这个电平转换收发器是必要的吗?可以去掉吗?
3. 手里一直在使用的leopardboard和Spectrum的368开发板上,将VDD_ISIF 18_33连接到了3.3V上,但是我看368datasheet上pin description中写道:
VDD_ISIF_18_33 power supply can be at 1.8V for VPFE pin functionality or it can be at 3.3V if other peripherals pin functionality is to be used like SPI3 or GPIO or CLKOUT0, or USBDRVVBUS.
我的理解是如果引脚功能是VPFE的话,那么VDD_ISIF 18_33应该连接1.8V的电源。可是为什么开发板都连接到了3.3V呢?
请大家帮忙,谢谢!