This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Am335x GPIO使用问题请教



大家好,

自己的开发板,GPMC_AD8~15作为输出,上电后8颗LED就立即会闪烁,此时没有跑任何code(我没有download 任何code)。

但是若一直reset的时候,它们是灭掉的;还有当我用CCS  connect  target成功后也可以灭掉,感觉奇怪!

 

线路中LED由OUT0~7控制,它们分别挂在 MCU的GPMC_AD8~15,LED闪烁也就是说 难道AD8~15会自动 拉高/拉低的变化吗??

将一个上拉电阻R379拿掉,重新上电还是会闪烁。            

  

所以,请问AD8~15这些脚位在上电后的状态 哪里 可以查询?

作为输出使用电路设计有问题么?

 谢谢!