希望各位可以帮帮忙。已经在论坛提问过很多次了,也请教过很多老师,仍然没有把这个问题解决,XDS200始终不能连接上电脑。
使用的是WIN7 x64操作系统,刚刚重装电脑并把CCS等软件全部重新装了一次,但是仍然和以前一样的错误;
USB接的是子卡上的miniUSB;
使用的是ccs5.5,驱动应该都默认在里面了,并且PC的设备管理器中能够正确识别XDS2xx,可见驱动应该无异常;
MCSDK也已经安装了,但是在CCS5.5包含NDK时出现错误;
SW3、5、9全部ON位;
J5是OPEN,J4无论是否OPEN都会出现这个问题;
XDS200上的LED,DS1,DS2一直亮起,可见XDS200的启动是成功的;
对提供的示例helloworld工程,新建了一个连接,目标 TI XDS2xx USB Onboard Emulator,Save后点击Test Connection出现以下错误:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -r -o -S pathlength -S integrity
[Result]
E_RPCENV_IO_ERROR(-6) No connection
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
但是如果USB接的是下面主板上的miniUSB口,并选择目标XDS100v1,是可以成功接上并且调试的。XDS200始终不行。