This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPNC DM385 更改视频输入接口



您好!我们想将IPNC DM385的sensor输入改为SDI/HDMI/YPbPr接口输入,请问三种接口改成何种接口输入开发难度最小?谢谢!

  • 你好,

    无论是哪种都需要外部芯片把信号转换为YUV422输入给DM385,难度取决于你对外部转换芯片的熟悉程度。

  • 您好!感谢您的回复。请问SDI芯片转化后的信号可以直接作为DM385的输入吗?

  • 你好,

      请查询DM385的手册,目前DM385支持内嵌同步的BT656格式,BT1120格式,以及外同步。请确认一下SDI芯片的输出信号与DM385的输入是否匹配。

  • Dear Chris Meng:

    您好!我们想输入HDMI 1.4接口的视频,然后传给DM385,经H.264 1080P 60fps 编码后,再无线发送视频码流。

    请问:

     (1)TI有没有HDMI 1.4的接口芯片?

     (2)如果我们购买了APPRO的DM385IPNC-AR0331摄像头后,利用其中的核心板,我们自己开发扩展板,实现包括视频采集和数据发送等功能,是否可行?appro公司有没有做加密或其他限制。因为我们不想用sensor,而是直接用摄像头的数据。

     (3)核心板再加上我们的扩展板,功耗大约会在多少瓦?

    谢谢!