This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

368与Micro-SD Card的连接问题



目前原理图画到368与Micro-SD Card的连接了。有一些问题想弄清楚。

上图是Leopardboard开发板上365与SD Card的连接(365与368是pin to pin的,所以用来参考)。我的问题是:

1. 为什么需要在DATA[0:4]数据线上串联10欧姆的排阻,排阻是否可以去掉?

2. 为什么需要在CLK和CMD串联33欧姆的电阻,串联电阻是否可以去掉?

3. 我发现368有2组SD卡接口,分别是SD0和SD1,在功能上这两组SD卡接口是否有区别?在决定使用哪一组时由什么来决定?随便用哪一组都可以吗?

下图是开发板上SD卡的电路。

我的问题是:

1. 为什么在DATA[0:4]和CLK上都加了51K的上拉电阻?

2. 为什么在CMD上却没有加上拉电阻(虚线框中的R55在电路板上没有焊接),反而加了510K的下拉电阻?

3. 上述两点中的上拉与下拉电阻是否可以去掉呢?

谢谢大家的帮助!