This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于edma接受串口数据的问题



现在正在调试用edma来实现串口数据的发送和接收,发送采取一块edma的方式,基本上的代码按照startware中的配置,可以实现循环的发送。在做接受的时候,使用ping-pong进行循环接收,接收也是基本上按照startware中的例子,edma配置的时候进行linkaddress的链接了,一块是uart1_rx的paRAM,另一块是第40块paRAM,现在的问题是只能进入一次接收中断,第二次就进不去了,TI的工程师有没有关于edma做ping-pong接收的例子,或者给予一点个人的建议?期待您的解答!

  • ping-pong传输中,使用两个两个paRAM是不够的,在OMAPL138中要使用三个。当一次EDMA传输完成后,链接paRAM中的数据将拷贝到串口通道paRAM中去,注意是拷贝,假如串口通道paRAM是ping接收,其Linker地址指向pong,pong接受的Linker指向另外一个链接ping  paRAM,这个链接ping paRAM的Linker地址再指向pong paRAM。这样说可能不清晰,你看手册sprugp9b.pdf  P.72页的例程。手册已经上传到附件中了。

    sprugp9b.pdf
  • 这个例程在omap_l138的手册里面也有,后来我就是按照手册上面的配置来配置paRAM,配置成为三块paRAM,但是进入两次中断之后就不会再产生中断了。是不是我的中断处理函数里面哪里没有清除,还是ping pong跑完之后需要手动重新配置ping pong的paRAM?

    我现在的配置是这样的,paRAM里面的opt按照手册上配置,只是把TCC改成了uart_rx,串口的parRAM链接到pong,其他都没有改变,然后另外两块parRAM是相互链接的,而且这个手册上我有一点不明白,就拿channel 3来说吧,它自己的paRAM中的opt配置为0x00103000,它link到第64块paRAM,但是第64块的paRAM中的opt为0x0010D000,这个数值我觉得有问题,既然是mcbsp了,为什么opt里面的tcc项又变成了D,D是表示uart1_tx,我现在是用edma的ping pong来做uart1_rx数据的接收,你能否给我正确的parRAM配置?

    还有一个疑问,中断处理跟普通的edma中断处理是一样的嘛?只要清楚IPR就可以了嘛?

  • #1:对于OPT的配置,三个paRAM都应该是一致的,ITCCHEN=1,使能内部传输完成级联;让TCC的值为12,16进制为C,这个代表EDMA传输完成后,会触发EVENT 12(UART1 Receive)所对应的EDMA中断。

             注:如果使用UART1 Receive,必须使用channel 12,其余的两个paRAM使用的channel大于64即可。

    #2:关于在EDMA中断中怎么清除中断标志位,这个在EDMA中有两组寄存器,分阴影部分和全局部分。如果搞不清除这两部分寄存器的区别时,建议使用全局部分寄存器,往ICR寄存器相应的位写1,就可以清除IPR中的相应的中断标志位了。