Part Number: OMAP-L138
请教一下,什么原因会导致在用OMAP-L138设计电路时发现当在E9脚(配置为上拉到3.3V,GPIO模式,输入,上升沿和下降沿响应中断)测量到一个1.3V左右电压时,处理器一直进中断,导致程序无法响应别的任务,电路如下。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OMAP-L138
请教一下,什么原因会导致在用OMAP-L138设计电路时发现当在E9脚(配置为上拉到3.3V,GPIO模式,输入,上升沿和下降沿响应中断)测量到一个1.3V左右电压时,处理器一直进中断,导致程序无法响应别的任务,电路如下。

断开与E9管脚的连接,用示波器测量HY_FLAG信号输出端,看HY_FLAG是不是正常的?如果输出是正常的,那就示波器同时测量HY_FLAG输出端和接收端E9管脚,看是不是一样的,不一样那就是HY_FLAG线路中受到了干扰。
只能硬件上排查看看。
测试未发现干扰,用外部直流源直接输入一个1.3V左右电压给HY_FLAG也会一直触发中断。IO口的逻辑电平在什么情况下会在1.3V左右震荡?