如下图所示:
上图是DM368的datasheet中描述的推荐电压工作范围。
其中VDDA12_DAC的描述为:1.2V Supply Voltage而后面却说范围为1.28V~1.42V,
我究竟是给1.2V呢?还是给1.35V呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请注意到这个图上面,特别注明了432MHz这个条件。
如果你打开DM365的手册,在相同的位置就是标注的是1.2V typical。
所以这个电压值实际是和频率相关的。