您好:我们的PCB设计中将C6416的引脚E16(BEA20)外部通过1K电阻拉高,在应用中出现大小端不稳定的现象,具体如下:
1、用台式机(1#)连接时,识别为小端,但是用万用表测量上啦电阻端的电压时,电压值小于400mV,但是C6416内部读数为1
2、用另一个台式机(2#)连接时,有时大端,有时小端
3、用第三台台式机连接时,一直为大端(外部实际上拉)
请您分析这是什么问题引起的?
补充说明:E16同时与FLASH的地址线(A20)连接
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.