This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CCSV5的一些问题

Other Parts Discussed in Thread: CCSTUDIO

最近狠 了一下心从CCS3.3升级到了CCS5.4,熟悉了一段时间后现在感觉很是郁闷,有几个问题求大家解答一下:

1.ccs3.3 中reset emulator 竟然消失了,取而代之的是debug按钮……现在CCS5.4经常出现连接仿真器失败的情况,我需要把CCS5.4关了,打开3.3,reset emulator 后再重新打开5.4,进行DEBUG。5.4没有类似的功能吗?

2.我把3.3的工程转成5.4的工程后,找不到新版本的工程在哪里……

3.都说CCSV5有烧写flash的功能,我想问一下怎么实现?我外挂的flash,烧写的话肯定需要配置地址,如何选择?


  • 1,在ccsv3.3中,仿真器的驱动是单独安装的,提供有Reset Emulator功能。

    Reset Emulator – Will reset the XDS and drive TRST- active, so the debug logic on chip is also reset. To make this command active the device must be disconnected by CCS.

    但ccsv5的仿真器驱动是集成在ccs中,没有单独发布。因此您“CCS5.4经常出现连接仿真器失败的情况”是什么错误信息,贴出来看看

  • 2,在ccsv5中,右键点击工程---属性----resource中,可以看到location。这里就是工程的地址所在。

  • 3,C6000的芯片内部都没有flash,是需要外挂flash芯片的。对flash的烧写都必须通过dsp的flash读写命令进行。需要建立一个这样的工程,CCS没有提供这样的工具。

  • 1.http://processors.wiki.ti.com/index.php/Emulation_Resets

    2.http://downloads.ti.com/dsps/dsps_public_sw/sdo_ccstudio/presentations/CCSv5-FromCCSv3.pdf

    3.http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/300616.aspx