目前用的是一个16BIT,128M的DDR2 SDRAM;
在DM368的datasheet中关于DDR的引脚描述部分有以下两个端口:
问题1:对于这两个端口的引脚描述。看的不是很明白,可以的话,麻烦解释一下。
问题2:同时datasheet中有如下描述:
下图是所参考的开发板原理图中的描述(较粗的红线是我后加的)。:
通过上面两幅图的描述的意思是:PCB布线时,上图中“粗红线”标出的长度要等与DDR时钟线和DDR数据线的长度。不知是否理解正确。
期待答案!谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.