各位专家们好!
请问利用EDMA3在EMIF和DDR3之间进行数据传输的时候,在程序中如何对EMIF进行正确的配置呢?由于我所用的C6678芯片的EMIF16和其他C6000系列的芯片的EMIF结构和寄存器都不一样,所以找不到可供参考的例子,请问能否提供EMIF16的参考配置程序呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thomas Yang
您好!我看到KeyStone_DDR_Init.c这个文件里面对DDR的初始化分为4种情况:TCI6608_EVM_DDR_Init(float clock_MHz);TCI6618_EVM_DDR_Init(float clock_MHz);TCI6614_VDB_DDR_Init(float clock_MHz);TCI6614_Huawei_DDR_Init(float clock_MHz),这4种情况分别针对4种DSP型号,我现在用的是C6678,和以上4种型号都一样,这是不是意味着不能根据这个程序来配置呢?如果可以的话那应该用哪一种呢?谢谢!
Andy Yin
我将您给的测试文件添加到新建的工程里面编译后,提示在C文件KeyStone_EMIF16_Init.c里有很多变量未定义,如下所示,我在程序中也确实找不到这些变量的定义,但是您给的例子里面是直接用的,请问是什么原因呢?是否是因为缺少某些头文件?谢谢!
identifier "CSL_EMIF16_AWCCR_CE0WAIT_MASK" is undefined
identifier "CSL_EMIF16_AWCCR_CE0WAIT_SHIFT" is undefined
identifier "CSL_EMIF16_NANDFCTL_CE0NAND_MASK" is undefined
identifier "CSL_EMIF16_NANDFCTL_CE0NAND_SHIFT" is undefined
identifier "CSL_EMIF16_PMCR_CE0PGDEL_MASK" is undefined
identifier "CSL_EMIF16_PMCR_CE0PGDEL_SHIFT" is undefined
identifier "CSL_EMIF16_PMCR_CE0PGMDEN_MASK" is undefined
identifier "CSL_EMIF16_PMCR_CE0PGMDEN_SHIFT" is undefined
identifier "CSL_EMIF16_PMCR_CE0PGSIZE_MASK" is undefined
identifier "CSL_EMIF16_PMCR_CE0PGSIZE_SHIFT" is undefined
我在测试自己的EMIF16外界Norflash时也遇到了这个问题,报错:
expression must have arithmetic or pointer type.
indentifier "CSL_Emif16_CFG_REGS " is undefined.
至于答复”这是由于该代码使用的CSL库是基于的TCI6614的,里面定义的宏名称和6678中的定义不同,请根据6678的csl库进行修改即可“——能否说的更详细点?直接举例说更好,非常感谢。
在6678的csl中搜索CSL_Emif16Regs,这个是在6678中定义的emif寄存器结构体的名字,把代码中的相关定义换掉就可以了,还有一些宏,类似CSL_EMIF16_A0CR_SS_SHIFT,也要替换。
请问C6678的csl库和其他C6000的csl库是不是一样的呢?还有就是C6678对应的lib文件应该在哪里去找呢?
专家你好,
我将csl宏定义更正,现在这部分没报错了(我将CE0改成CS2,这样对应正确么?比如CSL_EMIF16_AWCCR_CE0WAIT_SHIFT改成CSL_EMIF16_AWCCR_CS2WAIT_SHIFT,另外其他参数比如程序中的i也需要改么?)
现在我的程序仍有错误,如下所示
Description Resource Path Location Type
identifier "DEVICE_EMIF_NAND_ALE_OFFSET" is undefined flash_nand.c /EMIF/src/FLASH line 456 C/C++ Problem
identifier "DEVICE_EMIF_NAND_CLE_OFFSET" is undefined flash_nand.c /EMIF/src/FLASH line 451 C/C++ Problem
identifier "DEVICE_EMIF_NAND_DATA_OFFSET" is undefined flash_nand.c /EMIF/src/FLASH line 465 C/C++ Problem
identifier "DEVICE_EMIF_NAND_DATA_OFFSET" is undefined flash_nand.c /EMIF/src/FLASH line 507 C/C++ Problem
identifier "DEVICE_EMIF_NAND_DATA_OFFSET" is undefined flash_nand.c /EMIF/src/FLASH line 526 C/C++ Problem
identifier "DEVICE_EMIF_NAND_TIMEOUT" is undefined flash_nand.c /EMIF/src/FLASH line 122 C/C++ Problem
identifier "DEVICE_EMIF_NAND_TIMEOUT" is undefined flash_nand.c /EMIF/src/FLASH line 149 C/C++ Problem
identifier "DEVICE_EMIF_NAND_TIMEOUT" is undefined flash_nand.c /EMIF/src/FLASH line 285 C/C++ Problem
identifier "DEVICE_EMIF_NAND_TIMEOUT" is undefined flash_nand.c /EMIF/src/FLASH line 377 C/C++ Problem
struct "<unnamed>" has no field "NFECCCE0" flash_nand.c /EMIF/src/FLASH line 615 C/C++ Problem
但是比如我去源码中找,比如第一个提示错误NAND_ALE_OFFSET,因为调用了flash_nand.h, 所以是定义了的,能直接跳到
#define NAND_ALE_OFFSET DEVICE_EMIF_NAND_ALE_OFFSET, 但是为什么还会提示错误?
谢谢解答。