如下图所示,368晶振对参数有如下要求:
目前准备使用24MHz的Crysta
l如上图所示如果选择24M Crystal 要求ESR <=60ohm.
因为PCB板规划的面积有限,想选一颗封装比较小的Crystal,但小封装的Crystal的ESR有比较大,有200ohm,100ohm两种。
我的问题是ESR较大对368工作有影响吗?有什么影响?
我可以选择100ohm或200ohm的ESR 晶振吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.