各位专家好!
利用EDMA3在EMIF和DDR3之间进行数据传输的时候,能否采用事件触发?如果可以的话是否意味着在EDMA所有的通道事件中有和EMIF相关的某个事件,然后只需要对该事件对应的通道进行配置并等待事件产生以后触发通道传输即可?如果有的话那么是什么事件可以触发EDMA对EMIF的数据进行传输呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
andy lee,
在下面文档中的“Figure 2-2 EDMA3 Channel Controller (EDMA3CC) Block Diagram”,我们可以看到ESR/ESRH可以用来进行手动触发。