This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急求:C6678的DDR3扩展至8GB后内核与EDMA如何直接访问?



众所周知c6678的DDR3可以扩展到8GB,而keystone给DDR3分配的起始地址为0x80000000,地址空间大小只有2GB,请问把C6678的DDR3扩展的8GB后,内核和EDMA如何直接访问DDR3?

需要通过什么方式进行地址映射才能访问?

注:因算法的需要数据存储不是连续的,一次EDMA读取的数据地址跨度超过2GB,请问如何设置才能用EDMA直接访问?

有没相应的测试例程??