This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cmem错误



大家好:

我用的开发板是TI的dm6467,最近将自己编译的内核和根文件系统下载到开发板中,并成功启动了开发板。但是在运行loadmodules.sh文件时,却出现了如下的错误:

CMEMK Error: CMEM phys_start (0x82800000) overlaps kernel (0x80000000 -> 0x88000000)
insmod: error inserting 'cmemk.ko': -1 Invalid parameters
DSPLINK Module (1.64) created on Date: Jul 14 2010 Time: 15:39:32
load success !

当我运行自己的应用程序的时候,就会出现以下的错误:

CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
[CMEM_init fail]

请问各位,这是什么原因啊!谢谢