大家好,我使用dsp 6713,我在连接目标板时出现如下错误提示: :
: Error connecting to the target: :
: Error 0x80000200/-1070 : : Fatal Error during: OCS, : : An unknown error prevented the emulator from accessing the processor : : in a timely fashion. : : It is recommended to RESET EMULATOR. This will disconnect each : : target from the emulator. The targets should then be power cycled : : or hard reset followed by an emureset and reconnect to each target. : : Sequence ID: 0 : : Error Code: -1070 : : Error Class: 0x80000200 : : I/O Port = 240 : : Board Name: C671x TDS510USB 2.0 Emulator - WintechDigital : : Cpu Name: CPU_1 : : Abort: Close Code Composer Studio. : : Retry: Try to connect to the target again.
请各位老师看一下这个问题如何解决?