问题一:非连续存储的数据如何进行FFT变换?
需求说明:假如复数数组complex input[32768],我们想对input[32768]中每间隔3个复数的数据x进行fft变换,即x={input[0] input[4] input[8] input[12] ... input[32764] }组成的数据进行fft变化,有没有现成的函数可以调用???
如果有人已经实现了烦请上传一下测试历程。
问题二:DSPF_sp_fftSPxSP中的offset 的含义是什么?
能否用void DSPF_sp_fftSPxSP 实现问题一描述的功能
/* void DSPF_sp_fftSPxSP(
/* int N, float * ptr_x, float * ptr_w, float * ptr_y,
/* unsigned char * brev, int n_min, int offset, int n_max);
/*
/* N = length of fft in complex samples, power of 2 such that
/* N>=8 and N <= 16384.
/* ptr_x = pointer to complex data input
/* ptr_w = pointer to complex twiddle factor (see below)
/* ptr_y = pointer to complex output data
/* brev = pointer to bit reverse table containing 64 entries
/* n_min = smallest fft butterfly used in computation
/* used for decomposing fft into subffts, see notes
/* offset = index in complex samples of sub-fft from start of