做了8片DM8168的板子,其中有两片无法下载软件。
检测电源电压、上电时序、复位信号、时钟全部正常。通过网口从PC上下载Uboot。PC端软件提示下载成功。但是串口无法输出任何信息。用示波器看也没有任何波形从8168输出。
正常情况下,通过网口下载Uboot后,8168会跳到boot执行代码。之后会有log从串口输出。通过串口可以控制Uboot,然后进行配置,以及Flash烧写。有6片板子都正常。
这两片无法正常工作的板子可能是什么地方出了问题?DDR还是8168芯片本身已经损坏?或者是什么其他的问题。