This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

编译警告



CCS版本是5.4,出现如下警告,对程序运行有影响吗,谢谢!


**** Build of configuration Debug for project emif16_boot1 ****

"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building target: emif16_boot1.out'
'Invoking: C6000 Linker'
"C:/ti/ccsv5/tools/compiler/c6000_7.4.2/bin/cl6x" -mv6600 --abi=eabi -g --display_error_number --diag_warning=225 --diag_wrap=off -z -m"emif16_boot1.map" -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.2/lib" -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.2/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="emif16_boot1_linkInfo.xml" --rom_model -o "emif16_boot1.out" "./src/pll.obj" "./src/norflash.obj" "./src/main.obj" "./src/emif16.obj" "./boot.obj" -l"libc.a" "../boot.cmd"
<Linking>
warning #10278-D: LOAD placement specified for section ".text:decompress:none:__TI_decompress_none:rts6600_elf.lib<copy_decompress_none.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:memcpy:rts6600_elf.lib<memcpy64.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:decompress:rle24:__TI_decompress_rle24:rts6600_elf.lib<copy_decompress_rle.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section ".text:__TI_decompress_rle_core:rts6600_elf.lib<copy_decompress_rle.obj>". This section contains decompression routines required for linker generated copy tables and C/C++ auto-initialization. Must ensure that this section is copied to run address before the C/C++ boot code is executed or is placed with single allocation specifier (ex. "> MEMORY").
'Finished building target: emif16_boot1.out'
' '

**** Build Finished ****