This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678中DMA的种类



一直在和C66系列打交道,有些经验理解,和大家分享,可能会有些纰漏,欢迎探讨:)

IDMA:每个DSP内核带一个。C6678共8个

EDMA:一个C6678芯片内有三个组。 组1包含2个,组2、组3各包含4个,因此总共是10个。

PkDMA:这个是Multicore Navigator内部使用的DMA。


其中
-EDMA按照分组可以在所有内存空间L1,L2,SL2,DDR3进行拷贝。
-IDMA只能在L1,L2之间拷贝。
-PkDMA由Multicore Navigator操作拷贝。
-另外外设,EDMA,PA以及算法加速器等也会用到PkDMA。

欢迎探讨 William.dong@enea.com