This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x

Other Parts Discussed in Thread: TPS65217, TPS65910

最近在用ti的ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install调试板子,之前使用5.0版本。所以按照以前开发思路修改uboot.修改board.c文件中的read_eeprom()函数,告诉芯片是哪块开发板。代码如下

/*
* board.c
*
* Board functions for TI AM335X based boards
*
* Copyright (C) 2011, Texas Instruments, Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License as
* published by the Free Software Foundation; either version 2 of
* the License, or (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR /PURPOSE. See the
* GNU General Public License for more details.
*/

#include <common.h>
#include <errno.h>
#include <spl.h>
#include <asm/arch/cpu.h>
#include <asm/arch/hardware.h>
#include <asm/arch/omap.h>
#include <asm/arch/ddr_defs.h>
#include <asm/arch/clock.h>
#include <asm/arch/gpio.h>
#include <asm/arch/mmc_host_def.h>
#include <asm/arch/sys_proto.h>
#include <asm/io.h>
#include <asm/emif.h>
#include <asm/gpio.h>
#include <i2c.h>
#include <miiphy.h>
#include <cpsw.h>
#include "board.h"
#include "pmic.h"
#include "tps65217.h"

DECLARE_GLOBAL_DATA_PTR;

static struct wd_timer *wdtimer = (struct wd_timer *)WDT_BASE;
#if defined(CONFIG_SPL_BUILD) || (CONFIG_NOR_BOOT)
static struct uart_sys *uart_base = (struct uart_sys *)DEFAULT_UART_BASE;
#endif

/* MII mode defines */
#define MII_MODE_ENABLE 0x0
#define RGMII_MODE_ENABLE 0x3A
#define RMII_MODE_ENABLE 0x5

/* GPIO that controls power to DDR on EVM-SK */
#define GPIO_DDR_VTT_EN 7

static struct ctrl_dev *cdev = (struct ctrl_dev *)CTRL_DEVICE_BASE;

static struct am335x_baseboard_id __attribute__((section (".data"))) header;

static inline int board_is_bone(void)
{
return !strncmp(header.name, "A335BONE", HDR_NAME_LEN);
}

static inline int board_is_bone_lt(void)
{
return !strncmp(header.name, "A335BNLT", HDR_NAME_LEN);
}

static inline int board_is_evm_sk(void)
{
return !strncmp("A335X_SK", header.name, HDR_NAME_LEN);
}

static inline int board_is_idk(void)
{
return !strncmp(header.config, "SKU#02", 6);
}

static int __maybe_unused board_is_gp_evm(void)
{
return !strncmp("A33515BB", header.name, 8);
}

int board_is_evm_15_or_later(void)
{
return (!strncmp("A33515BB", header.name, 8) &&
strncmp("1.5", header.version, 3) <= 0);
}

/*
* Read header information from EEPROM into global structure.
*/
static int read_eeprom(void)
{
#if 0
/* Check if baseboard eeprom is available */
if (i2c_probe(CONFIG_SYS_I2C_EEPROM_ADDR)) {
puts("Could not probe the EEPROM; something fundamentally "
"wrong on the I2C bus.\n");
return -ENODEV;
}

/* read the eeprom using i2c */
if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 2, (uchar *)&header,
sizeof(header))) {
puts("Could not read the EEPROM; something fundamentally"
" wrong on the I2C bus.\n");
return -EIO;
}
#endif

header.magic = 0xEE3355AA;
strcpy(header.version,"1.2B");
strcpy(header.serial,"mxz");
printf("header.version = %s\n",header.version);
printf("header.name = %s\n",header.name);
strcpy(header.name,"A335X_SK");
printf("header.name = %s\n",header.name);
printf("header.version = %s\n",header.version);

printf("header.name = %s\n",header.name);
#if 0
if (header.magic != 0xEE3355AA) {
/*
* read the eeprom using i2c again,
* but use only a 1 byte address
*/
if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
(uchar *)&header, sizeof(header))) {
puts("Could not read the EEPROM; something "
"fundamentally wrong on the I2C bus.\n");
return -EIO;
}

if (header.magic != 0xEE3355AA) {
printf("Incorrect magic number (0x%x) in EEPROM\n",
header.magic);
return -EINVAL;
}
}
#endif
return 0;
}

/* UART Defines */
#if defined(CONFIG_SPL_BUILD) || defined(CONFIG_NOR_BOOT)
/**
* tps65217_reg_read() - Generic function that can read a TPS65217 register
* @src_reg: Source register address
* @src_val: Address of destination variable
*/

unsigned char tps65217_reg_read(uchar src_reg, uchar *src_val)
{
if (i2c_read(TPS65217_CHIP_PM, src_reg, 1, src_val, 1))
return 1;
return 0;
}

/**
* tps65217_reg_write() - Generic function that can write a TPS65217 PMIC
* register or bit field regardless of protection
* level.
*
* @prot_level: Register password protection.
* use PROT_LEVEL_NONE, PROT_LEVEL_1, or PROT_LEVEL_2
* @dest_reg: Register address to write.
* @dest_val: Value to write.
* @mask: Bit mask (8 bits) to be applied. Function will only
* change bits that are set in the bit mask.
*
* @return: 0 for success, 1 for failure.
*/
int tps65217_reg_write(uchar prot_level, uchar dest_reg,
uchar dest_val, uchar mask)
{
uchar read_val;
uchar xor_reg;

/* if we are affecting only a bit field, read dest_reg and apply the mask */
if (mask != MASK_ALL_BITS) {
if (i2c_read(TPS65217_CHIP_PM, dest_reg, 1, &read_val, 1))
return 1;
read_val &= (~mask);
read_val |= (dest_val & mask);
dest_val = read_val;
}

if (prot_level > 0) {
xor_reg = dest_reg ^ PASSWORD_UNLOCK;
if (i2c_write(TPS65217_CHIP_PM, PASSWORD, 1, &xor_reg, 1))
return 1;
}

if (i2c_write(TPS65217_CHIP_PM, dest_reg, 1, &dest_val, 1))
return 1;

if (prot_level == PROT_LEVEL_2) {
if (i2c_write(TPS65217_CHIP_PM, PASSWORD, 1, &xor_reg, 1))
return 1;

if (i2c_write(TPS65217_CHIP_PM, dest_reg, 1, &dest_val, 1))
return 1;
}

return 0;
}

int tps65217_voltage_update(unsigned char dc_cntrl_reg, unsigned char volt_sel)
{
if ((dc_cntrl_reg != DEFDCDC1) && (dc_cntrl_reg != DEFDCDC2)
&& (dc_cntrl_reg != DEFDCDC3))
return 1;

/* set voltage level */
if (tps65217_reg_write(PROT_LEVEL_2, dc_cntrl_reg, volt_sel, MASK_ALL_BITS))
return 1;

/* set GO bit to initiate voltage transition */
if (tps65217_reg_write(PROT_LEVEL_2, DEFSLEW, DCDC_GO, DCDC_GO))
return 1;

return 0;
}

/*
* voltage switching for MPU frequency switching.
* @module = mpu - 0, core - 1
* @vddx_op_vol_sel = vdd voltage to set
*/

#define MPU 0
#define CORE 1

int voltage_update(unsigned int module, unsigned char vddx_op_vol_sel)
{
uchar buf[4];
unsigned int reg_offset;

if(module == MPU)
reg_offset = PMIC_VDD1_OP_REG;
else
reg_offset = PMIC_VDD2_OP_REG;

/* Select VDDx OP */
if (i2c_read(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
return 1;

buf[0] &= ~PMIC_OP_REG_CMD_MASK;

if (i2c_write(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
return 1;

/* Configure VDDx OP Voltage */
if (i2c_read(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
return 1;

buf[0] &= ~PMIC_OP_REG_SEL_MASK;
buf[0] |= vddx_op_vol_sel;

if (i2c_write(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
return 1;

if (i2c_read(PMIC_CTRL_I2C_ADDR, reg_offset, 1, buf, 1))
return 1;

if ((buf[0] & PMIC_OP_REG_SEL_MASK ) != vddx_op_vol_sel)
return 1;

return 0;
}

#define UART_RESET (0x1 << 1)
#define UART_CLK_RUNNING_MASK 0x1
#define UART_SMART_IDLE_EN (0x1 << 0x3)

static void rtc32k_enable(void)
{
struct rtc_regs *rtc = (struct rtc_regs *)AM335X_RTC_BASE;

/*
* Unlock the RTC's registers. For more details please see the
* RTC_SS section of the TRM. In order to unlock we need to
* write these specific values (keys) in this order.
*/
writel(0x83e70b13, &rtc->kick0r);
writel(0x95a4f1e0, &rtc->kick1r);

/* Enable the RTC 32K OSC by setting bits 3 and 6. */
writel((1 << 3) | (1 << 6), &rtc->osc);
}

static const struct ddr_data ddr2_data = {
.datardsratio0 = ((MT47H128M16RT25E_RD_DQS<<30) |
(MT47H128M16RT25E_RD_DQS<<20) |
(MT47H128M16RT25E_RD_DQS<<10) |
(MT47H128M16RT25E_RD_DQS<<0)),
.datawdsratio0 = ((MT47H128M16RT25E_WR_DQS<<30) |
(MT47H128M16RT25E_WR_DQS<<20) |
(MT47H128M16RT25E_WR_DQS<<10) |
(MT47H128M16RT25E_WR_DQS<<0)),
.datawiratio0 = ((MT47H128M16RT25E_PHY_WRLVL<<30) |
(MT47H128M16RT25E_PHY_WRLVL<<20) |
(MT47H128M16RT25E_PHY_WRLVL<<10) |
(MT47H128M16RT25E_PHY_WRLVL<<0)),
.datagiratio0 = ((MT47H128M16RT25E_PHY_GATELVL<<30) |
(MT47H128M16RT25E_PHY_GATELVL<<20) |
(MT47H128M16RT25E_PHY_GATELVL<<10) |
(MT47H128M16RT25E_PHY_GATELVL<<0)),
.datafwsratio0 = ((MT47H128M16RT25E_PHY_FIFO_WE<<30) |
(MT47H128M16RT25E_PHY_FIFO_WE<<20) |
(MT47H128M16RT25E_PHY_FIFO_WE<<10) |
(MT47H128M16RT25E_PHY_FIFO_WE<<0)),
.datawrsratio0 = ((MT47H128M16RT25E_PHY_WR_DATA<<30) |
(MT47H128M16RT25E_PHY_WR_DATA<<20) |
(MT47H128M16RT25E_PHY_WR_DATA<<10) |
(MT47H128M16RT25E_PHY_WR_DATA<<0)),
.datauserank0delay = MT47H128M16RT25E_PHY_RANK0_DELAY,
.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct cmd_control ddr2_cmd_ctrl_data = {
.cmd0csratio = MT47H128M16RT25E_RATIO,
.cmd0dldiff = MT47H128M16RT25E_DLL_LOCK_DIFF,
.cmd0iclkout = MT47H128M16RT25E_INVERT_CLKOUT,

.cmd1csratio = MT47H128M16RT25E_RATIO,
.cmd1dldiff = MT47H128M16RT25E_DLL_LOCK_DIFF,
.cmd1iclkout = MT47H128M16RT25E_INVERT_CLKOUT,

.cmd2csratio = MT47H128M16RT25E_RATIO,
.cmd2dldiff = MT47H128M16RT25E_DLL_LOCK_DIFF,
.cmd2iclkout = MT47H128M16RT25E_INVERT_CLKOUT,
};

static const struct emif_regs ddr2_emif_reg_data = {
.sdram_config = MT47H128M16RT25E_EMIF_SDCFG,
.ref_ctrl = MT47H128M16RT25E_EMIF_SDREF,
.sdram_tim1 = MT47H128M16RT25E_EMIF_TIM1,
.sdram_tim2 = MT47H128M16RT25E_EMIF_TIM2,
.sdram_tim3 = MT47H128M16RT25E_EMIF_TIM3,
.emif_ddr_phy_ctlr_1 = MT47H128M16RT25E_EMIF_READ_LATENCY,
};

static const struct ddr_data ddr3_data = {
.datardsratio0 = MT41J128MJT125_RD_DQS,
.datawdsratio0 = MT41J128MJT125_WR_DQS,
.datafwsratio0 = MT41J128MJT125_PHY_FIFO_WE,
.datawrsratio0 = MT41J128MJT125_PHY_WR_DATA,
.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct ddr_data ddr3_beagleblack_data = {
.datardsratio0 = MT41K256M16HA125E_RD_DQS,
.datawdsratio0 = MT41K256M16HA125E_WR_DQS,
.datafwsratio0 = MT41K256M16HA125E_PHY_FIFO_WE,
.datawrsratio0 = MT41K256M16HA125E_PHY_WR_DATA,
.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct ddr_data ddr3_evm_data = {
.datardsratio0 = MT41J512M8RH125_RD_DQS,
.datawdsratio0 = MT41J512M8RH125_WR_DQS,
.datafwsratio0 = MT41J512M8RH125_PHY_FIFO_WE,
.datawrsratio0 = MT41J512M8RH125_PHY_WR_DATA,
.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct cmd_control ddr3_cmd_ctrl_data = {
.cmd0csratio = MT41J128MJT125_RATIO,
.cmd0dldiff = MT41J128MJT125_DLL_LOCK_DIFF,
.cmd0iclkout = MT41J128MJT125_INVERT_CLKOUT,

.cmd1csratio = MT41J128MJT125_RATIO,
.cmd1dldiff = MT41J128MJT125_DLL_LOCK_DIFF,
.cmd1iclkout = MT41J128MJT125_INVERT_CLKOUT,

.cmd2csratio = MT41J128MJT125_RATIO,
.cmd2dldiff = MT41J128MJT125_DLL_LOCK_DIFF,
.cmd2iclkout = MT41J128MJT125_INVERT_CLKOUT,
};

static const struct cmd_control ddr3_beagleblack_cmd_ctrl_data = {
.cmd0csratio = MT41K256M16HA125E_RATIO,
.cmd0dldiff = MT41K256M16HA125E_DLL_LOCK_DIFF,
.cmd0iclkout = MT41K256M16HA125E_INVERT_CLKOUT,

.cmd1csratio = MT41K256M16HA125E_RATIO,
.cmd1dldiff = MT41K256M16HA125E_DLL_LOCK_DIFF,
.cmd1iclkout = MT41K256M16HA125E_INVERT_CLKOUT,

.cmd2csratio = MT41K256M16HA125E_RATIO,
.cmd2dldiff = MT41K256M16HA125E_DLL_LOCK_DIFF,
.cmd2iclkout = MT41K256M16HA125E_INVERT_CLKOUT,
};

static const struct cmd_control ddr3_evm_cmd_ctrl_data = {
.cmd0csratio = MT41J512M8RH125_RATIO,
.cmd0dldiff = MT41J512M8RH125_DLL_LOCK_DIFF,
.cmd0iclkout = MT41J512M8RH125_INVERT_CLKOUT,

.cmd1csratio = MT41J512M8RH125_RATIO,
.cmd1dldiff = MT41J512M8RH125_DLL_LOCK_DIFF,
.cmd1iclkout = MT41J512M8RH125_INVERT_CLKOUT,

.cmd2csratio = MT41J512M8RH125_RATIO,
.cmd2dldiff = MT41J512M8RH125_DLL_LOCK_DIFF,
.cmd2iclkout = MT41J512M8RH125_INVERT_CLKOUT,
};

static struct emif_regs ddr3_emif_reg_data = {
.sdram_config = MT41J128MJT125_EMIF_SDCFG,
.ref_ctrl = MT41J128MJT125_EMIF_SDREF,
.sdram_tim1 = MT41J128MJT125_EMIF_TIM1,
.sdram_tim2 = MT41J128MJT125_EMIF_TIM2,
.sdram_tim3 = MT41J128MJT125_EMIF_TIM3,
.zq_config = MT41J128MJT125_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41J128MJT125_EMIF_READ_LATENCY |
PHY_EN_DYN_PWRDN,
};

static struct emif_regs ddr3_beagleblack_emif_reg_data = {
.sdram_config = MT41K256M16HA125E_EMIF_SDCFG,
.ref_ctrl = MT41K256M16HA125E_EMIF_SDREF,
.sdram_tim1 = MT41K256M16HA125E_EMIF_TIM1,
.sdram_tim2 = MT41K256M16HA125E_EMIF_TIM2,
.sdram_tim3 = MT41K256M16HA125E_EMIF_TIM3,
.zq_config = MT41K256M16HA125E_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41K256M16HA125E_EMIF_READ_LATENCY |
PHY_EN_DYN_PWRDN,
};

static struct emif_regs ddr3_evm_emif_reg_data = {
.sdram_config = MT41J512M8RH125_EMIF_SDCFG,
.ref_ctrl = MT41J512M8RH125_EMIF_SDREF,
.sdram_tim1 = MT41J512M8RH125_EMIF_TIM1,
.sdram_tim2 = MT41J512M8RH125_EMIF_TIM2,
.sdram_tim3 = MT41J512M8RH125_EMIF_TIM3,
.zq_config = MT41J512M8RH125_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41J512M8RH125_EMIF_READ_LATENCY |
PHY_EN_DYN_PWRDN,
};

void am33xx_spl_board_init(void)
{
int mpu_vdd, mpu_pll, sil_rev;
printf("am33xx_spl_board_init\n");

/* Assume PG 1.0 */
mpu_pll = MPUPLL_M_720;

sil_rev = readl(&cdev->deviceid) >> 28;
printf("sil_rev = %d\n",sil_rev);
if (sil_rev == 1)
/* PG 2.0, efuse may not be set. */
mpu_pll = MPUPLL_M_800;
else if (sil_rev >= 2) {
/* Check what the efuse says our max speed is. */
int efuse_arm_mpu_max_freq;
efuse_arm_mpu_max_freq = readl(&cdev->efuse_sma);
if ((efuse_arm_mpu_max_freq & DEVICE_ID_MASK) ==
AM335X_ZCZ_1000)
mpu_pll = MPUPLL_M_1000;
else if ((efuse_arm_mpu_max_freq & DEVICE_ID_MASK) ==
AM335X_ZCZ_800)
mpu_pll = MPUPLL_M_800;
}

/*
* HACK: PG 2.0 should have max of 800MHz but Beaglebone Black
* can work at 1GHz.
*/
if (board_is_bone_lt())
mpu_pll = MPUPLL_M_1000;

if (board_is_bone() || board_is_bone_lt()) {
/* BeagleBone PMIC Code */
uchar pmic_status_reg;
int usb_cur_lim;

/* Only perform PMIC configurations if board rev > A1 */
if (board_is_bone() && !strncmp(header.version, "00A1", 4))
return;

if (i2c_probe(TPS65217_CHIP_PM))
return;

if (tps65217_reg_read(STATUS, &pmic_status_reg))
return;

/*
* Increase USB current limit to 1300mA or 1800mA and set
* the MPU voltage controller as needed.
*/
if (mpu_pll == MPUPLL_M_1000) {
usb_cur_lim = USB_INPUT_CUR_LIMIT_1800MA;
mpu_vdd = DCDC_VOLT_SEL_1325MV;
} else {
usb_cur_lim = USB_INPUT_CUR_LIMIT_1300MA;
mpu_vdd = DCDC_VOLT_SEL_1275MV;
}

if (tps65217_reg_write(PROT_LEVEL_NONE, POWER_PATH,
usb_cur_lim, USB_INPUT_CUR_LIMIT_MASK))
printf("tps65217_reg_write failure\n");

/* Set DCDC3 (CORE) voltage to 1.125V */
if (tps65217_voltage_update(DEFDCDC3, DCDC_VOLT_SEL_1125MV)) {
printf("tps65217_voltage_update failure\n");
return;
}

/* Set CORE Frequency to what we detected */
core_pll_config(OPP_100);

/* Set DCDC2 (MPU) voltage to 1.275V */
if (tps65217_voltage_update(DEFDCDC2, mpu_vdd)) {
printf("tps65217_voltage_update failure\n");
return;
}

/* Set MPU Frequency to what we detected */
mpu_pll_config(mpu_pll);

/*
* Set LDO3, LDO4 output voltage to 3.3V for Beaglebone.
* Set LDO3 to 1.8V and LDO4 to 3.3V for Beaglebone Black.
*/
if (board_is_bone()) {
if (tps65217_reg_write(PROT_LEVEL_2, DEFLS1,
LDO_VOLTAGE_OUT_3_3, LDO_MASK))
printf("tps65217_reg_write failure\n");
} else {
if (tps65217_reg_write(PROT_LEVEL_2, DEFLS1,
LDO_VOLTAGE_OUT_1_8, LDO_MASK))
printf("tps65217_reg_write failure\n");
}

if (tps65217_reg_write(PROT_LEVEL_2, DEFLS2,
LDO_VOLTAGE_OUT_3_3, LDO_MASK))
printf("tps65217_reg_write failure\n");

/* Only Beaglebone needs the AC power, not Beaglebone Black */
if (board_is_bone() &&
!(pmic_status_reg & PWR_SRC_AC_BITMASK)) {
printf("No AC power, disabling frequency switch\n");
return;
}
} else {
uchar buf[4];

/*
* The GP EVM, IDK and EVM SK use a TPS65910 PMIC. For all
* MPU frequencies we support we use a CORE voltage of
* 1.1375V. For 1GHz we need to use an MPU voltage of
* 1.3250V and for 720MHz or 800MHz we use 1.2625V.
*/
if (i2c_probe(PMIC_CTRL_I2C_ADDR))
return;

/* VDD1/2 voltage selection register access by control i/f */
if (i2c_read(PMIC_CTRL_I2C_ADDR, PMIC_DEVCTRL_REG, 1, buf, 1))
return;

buf[0] |= PMIC_DEVCTRL_REG_SR_CTL_I2C_SEL_CTL_I2C;

if (i2c_write(PMIC_CTRL_I2C_ADDR, PMIC_DEVCTRL_REG, 1, buf, 1))
return;

/*
* Unless we're running at 1GHz we use thesame VDD for
* all other frequencies we switch to (currently 720MHz,
* 800MHz or 1GHz).
*/
if (mpu_pll == MPUPLL_M_1000)
mpu_vdd = PMIC_OP_REG_SEL_1_3_2_5;
else
mpu_vdd = PMIC_OP_REG_SEL_1_2_6;

if (!voltage_update(CORE, PMIC_OP_REG_SEL_1_1_3))
core_pll_config(OPP_100);
if (!voltage_update(MPU, mpu_vdd))
mpu_pll_config(mpu_pll);
}
}
#endif

/*
* early system init of muxing and clocks.
*/
void s_init(void)
{
printf("s_init\n");
__maybe_unused struct am335x_baseboard_id header;
#ifdef CONFIG_NOR_BOOT
asm("stmfd sp!, {r2 - r4}");
asm("movw r4, #0x8A4");
asm("movw r3, #0x44E1");
asm("orr r4, r4, r3, lsl #16");
asm("mov r2, #9");
asm("mov r3, #8");
asm("gpmc_mux: str r2, [r4], #4");
asm("subs r3, r3, #1");
asm("bne gpmc_mux");
asm("ldmfd sp!, {r2 - r4}");
#endif

/* WDT1 is already running when the bootloader gets control
* Disable it to avoid "random" resets
*/
writel(0xAAAA, &wdtimer->wdtwspr);
while (readl(&wdtimer->wdtwwps) != 0x0)
;
writel(0x5555, &wdtimer->wdtwspr);
while (readl(&wdtimer->wdtwwps) != 0x0)
;

#if defined(CONFIG_SPL_BUILD) || defined(CONFIG_NOR_BOOT)
/* Setup the PLLs and the clocks for the peripherals */
pll_init();

/* Enable RTC32K clock */
rtc32k_enable();

/* UART softreset */
u32 regVal;

#ifdef CONFIG_SERIAL1
printf("enable_uart0_pin_mux\n");
enable_uart0_pin_mux();
#endif /* CONFIG_SERIAL1 */
#if 0
#ifdef CONFIG_SERIAL2
enable_uart1_pin_mux();
#endif /* CONFIG_SERIAL2 */
#ifdef CONFIG_SERIAL3
enable_uart2_pin_mux();
#endif /* CONFIG_SERIAL3 */
#ifdef CONFIG_SERIAL4
enable_uart3_pin_mux();
#endif /* CONFIG_SERIAL4 */
#ifdef CONFIG_SERIAL5
enable_uart4_pin_mux();
#endif /* CONFIG_SERIAL5 */
#ifdef CONFIG_SERIAL6
enable_uart5_pin_mux();
#endif /* CONFIG_SERIAL6 */
#endif
regVal = readl(&uart_base->uartsyscfg);
regVal |= UART_RESET;
writel(regVal, &uart_base->uartsyscfg);
while ((readl(&uart_base->uartsyssts) &
UART_CLK_RUNNING_MASK) != UART_CLK_RUNNING_MASK)
;

/* Disable smart idle */
regVal = readl(&uart_base->uartsyscfg);
regVal |= UART_SMART_IDLE_EN;
writel(regVal, &uart_base->uartsyscfg);

#if defined(CONFIG_NOR_BOOT)
printf("CONFIG_NOR_BOOT\n");
gd = (gd_t *) ((CONFIG_SYS_INIT_SP_ADDR) & ~0x07);
gd->baudrate = CONFIG_BAUDRATE;
serial_init();
gd->have_console = 1;
#else
gd = &gdata;

preloader_console_init();
#endif

/* Initalize the board header */
enable_i2c0_pin_mux();
i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
#ifndef CONFIG_NOR_BOOT
printf("read_eeprom\n");
if (read_eeprom() < 0)
puts("Could not get board ID.\n");
printf("header.name = %s\n",header.name);
#endif
#if 0
/* Check if baseboard eeprom is available */
if (i2c_probe(CONFIG_SYS_I2C_EEPROM_ADDR)) {
puts("Could not probe the EEPROM; something fundamentally "
"wrong on the I2C bus.\n");
}

/* read the eeprom using i2c */
if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 2, (uchar *)&header,
sizeof(header))) {
puts("Could not read the EEPROM; something fundamentally"
" wrong on the I2C bus.\n");
}
#endif
#if 0
if (header.magic != 0xEE3355AA) {
/*
* read the eeprom using i2c again,
* but use only a 1 byte address
*/
if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
(uchar *)&header, sizeof(header))) {
puts("Could not read the EEPROM; something "
"fundamentally wrong on the I2C bus.\n");
hang();
}

if (header.magic != 0xEE3355AA) {
printf("Incorrect magic number (0x%x) in EEPROM\n",
header.magic);
hang();
}
}
#endif
printf("header.name = %s\n",header.name);
enable_board_pin_mux(&header);
printf("enable_board_pin_mux(&header)\n");
printf("header.name = %s\n",header.name);
if (!strncmp("A335X_SK", header.name, HDR_NAME_LEN)) {
/*
* EVM SK 1.2A and later use gpio0_7 to enable DDR3.
* This is safe enough to do on older revs.
*/
printf("!strncmp header.name, HDR_NAME_LEN)\n");
gpio_request(GPIO_DDR_VTT_EN, "ddr_vtt_en");
gpio_direction_output(GPIO_DDR_VTT_EN, 1);
}

#ifdef CONFIG_NOR_BOOT
printf("CONFIG_NOR_BOOT\n");
am33xx_spl_board_init();
#endif

if (!strncmp("A335X_SK", header.name, HDR_NAME_LEN))
{
config_ddr(303, MT41J128MJT125_IOCTRL_VALUE, &ddr3_data,
&ddr3_cmd_ctrl_data, &ddr3_emif_reg_data);
printf("config_ddr\n");
}
else if (!strncmp("A335BNLT", header.name, 8))
config_ddr(400, MT41K256M16HA125E_IOCTRL_VALUE,
&ddr3_beagleblack_data,
&ddr3_beagleblack_cmd_ctrl_data,
&ddr3_beagleblack_emif_reg_data);
else if (!strncmp("A33515BB", header.name, 8) &&
strncmp("1.5", header.version, 3) <= 0)
config_ddr(303, MT41J512M8RH125_IOCTRL_VALUE, &ddr3_evm_data,
&ddr3_evm_cmd_ctrl_data, &ddr3_evm_emif_reg_data);
else
config_ddr(266, MT47H128M16RT25E_IOCTRL_VALUE, &ddr2_data,
&ddr2_cmd_ctrl_data, &ddr2_emif_reg_data);
#endif
}

/*
* Basic board specific setup. Pinmux has been handled already.
*/
int board_init(void)
{
i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
if (read_eeprom() < 0)
puts("Could not get board ID.\n");

gd->bd->bi_boot_params = PHYS_DRAM_1 + 0x100;

gpmc_init();

return 0;
}

#ifdef CONFIG_BOARD_LATE_INIT
int board_late_init(void)
{
#ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
char safe_string[HDR_NAME_LEN + 1];

/* Now set variables based on the header. */
strncpy(safe_string, (char *)header.name, sizeof(header.name));
safe_string[sizeof(header.name)] = 0;
setenv("board_name", safe_string);

strncpy(safe_string, (char *)header.version, sizeof(header.version));
safe_string[sizeof(header.version)] = 0;
setenv("board_rev", safe_string);
#endif

return 0;
}
#endif

#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
static void cpsw_control(int enabled)
{
/* VTP can be added here */

return;
}

static struct cpsw_slave_data cpsw_slaves[] = {
{
.slave_reg_ofs = 0x208,
.sliver_reg_ofs = 0xd80,
.phy_id = 1,
},
{
.slave_reg_ofs = 0x308,
.sliver_reg_ofs = 0xdc0,
.phy_id = 3,
},
};

static struct cpsw_platform_data cpsw_data = {
.mdio_base = AM335X_CPSW_MDIO_BASE,
.cpsw_base = AM335X_CPSW_BASE,
.mdio_div = 0xff,
.channels = 8,
.cpdma_reg_ofs = 0x800,
.slaves = 2,
.slave_data = cpsw_slaves,
.ale_reg_ofs = 0xd00,
.ale_entries = 1024,
.host_port_reg_ofs = 0x108,
.hw_stats_reg_ofs = 0x900,
.mac_control = (1 << 5),
.control = cpsw_control,
.host_port_num = 0,
.version = CPSW_CTRL_VERSION_2,
};
#endif

#if defined(CONFIG_DRIVER_TI_CPSW) || \
(defined(CONFIG_USB_ETHER) && defined(CONFIG_MUSB_GADGET))
int board_eth_init(bd_t *bis)
{
int rv, n = 0;
uint8_t mac_addr[6];
uint32_t mac_hi, mac_lo;

/* try reading mac address from efuse */
mac_lo = readl(&cdev->macid0l);
mac_hi = readl(&cdev->macid0h);
mac_addr[0] = mac_hi & 0xFF;
mac_addr[1] = (mac_hi & 0xFF00) >> 8;
mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
mac_addr[4] = mac_lo & 0xFF;
mac_addr[5] = (mac_lo & 0xFF00) >> 8;

#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
if (!getenv("ethaddr")) {
printf("<ethaddr> not set. Validating first E-fuse MAC\n");

if (is_valid_ether_addr(mac_addr))
eth_setenv_enetaddr("ethaddr", mac_addr);
}
#if 0
if (board_is_bone() || board_is_bone_lt() || board_is_idk()) {
writel(MII_MODE_ENABLE, &cdev->miisel);
cpsw_slaves[0].phy_if = cpsw_slaves[1].phy_if =
PHY_INTERFACE_MODE_MII;
} else {
writel(RGMII_MODE_ENABLE, &cdev->miisel);
cpsw_slaves[0].phy_if = cpsw_slaves[1].phy_if =
PHY_INTERFACE_MODE_RGMII;
}
#endif
writel(RMII_MODE_ENABLE|(3<<6),&cdev->miisel);
cpsw_slaves[0].phy_if = cpsw_slaves[1].phy_if =
PHY_INTERFACE_MODE_RMII;
rv = cpsw_register(&cpsw_data);
if (rv < 0)
printf("Error %d registering CPSW switch\n", rv);
else
n += rv;

/*
*
* CPSW RGMII Internal Delay Mode is not supported in all PVT
* operating points. So we must set the TX clock delay feature
* in the AR8051 PHY. Since we only support a single ethernet
* device in U-Boot, we only do this for the first instance.
*/
#if 0
#define AR8051_PHY_DEBUG_ADDR_REG 0x1d
#define AR8051_PHY_DEBUG_DATA_REG 0x1e
#define AR8051_DEBUG_RGMII_CLK_DLY_REG 0x5
#define AR8051_RGMII_TX_CLK_DLY 0x100

if (board_is_evm_sk() || board_is_gp_evm()) {
const char *devname;
devname = miiphy_get_current_dev();

miiphy_write(devname, 0x0, AR8051_PHY_DEBUG_ADDR_REG,
AR8051_DEBUG_RGMII_CLK_DLY_REG);
miiphy_write(devname, 0x0, AR8051_PHY_DEBUG_DATA_REG,
AR8051_RGMII_TX_CLK_DLY);
}
#endif
#endif
#if defined(CONFIG_USB_ETHER) && \
(!defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_USBETH_SUPPORT))
if (is_valid_ether_addr(mac_addr))
eth_setenv_enetaddr("usbnet_devaddr", mac_addr);

rv = usb_eth_initialize(bis);
if (rv < 0)
printf("Error %d registering USB_ETHER\n", rv);
else
n += rv;
#endif
return n;
}
#endif

主要修改read_eeprom中内容,认为给header赋值,但是串口打印信息非常奇怪

如下 :

U-Boot SPL 2013.01.01 (May 29 2014 - 05:13:59)
read_eeprom
header.version = 1.2Bmxz
header.name =
header.name = A335X_SK
header.version =
header.name = A335X_SK
header.name =
header.name =
enable_board_pin_mux
enable_board_pin_mux(&header)
header.name =

通过打印信息可得,header.name没有赋值成功,导致程序无法判断是哪块开发板,检查无数遍,没有问题,求详解,歇息

  • 我之前改 read_eeprom(void) 也是無效

    後來改這樣就OK

    void am33xx_spl_board_init(void)
    {
    int mpu_vdd, mpu_pll, sil_rev;

    /* Assume PG 1.0 */
    mpu_pll = MPUPLL_M_720;

    sil_rev = readl(&cdev->deviceid) >> 28;
    if (sil_rev == 1)
    /* PG 2.0, efuse may not be set. */
    mpu_pll = MPUPLL_M_800;
    else if (sil_rev >= 2) {
    /* Check what the efuse says our max speed is. */
    int efuse_arm_mpu_max_freq;
    efuse_arm_mpu_max_freq = readl(&cdev->efuse_sma);
    if ((efuse_arm_mpu_max_freq & DEVICE_ID_MASK) ==
    AM335X_ZCZ_1000)
    mpu_pll = MPUPLL_M_1000;
    else if ((efuse_arm_mpu_max_freq & DEVICE_ID_MASK) ==
    AM335X_ZCZ_800)
    mpu_pll = MPUPLL_M_800;
    }

    #if 1 
    header.magic = 0xEE3355AA;
    strcpy(header.name, "A335X_SK");//strcpy(header.name, "A335BNLT");
    strcpy(header.version, "1.2B");//strcpy(header.version, "00A6");
    strcpy(header.serial, "45124P196447");//strcpy(header.serial, "4313BBBK1325");
    strcpy(header.config, "SKU#00");
    header.mac_addr[0][0]=0x11;
    header.mac_addr[0][1]=0x22;
    header.mac_addr[0][2]=0x33;
    header.mac_addr[0][3]=0x44;
    header.mac_addr[0][4]=0x55;
    header.mac_addr[0][5]=0x66;
    #endif

    .....


    void s_init(void)

    ...

    #if 0

    #ifndef CONFIG_NOR_BOOT
    if (read_eeprom() < 0)
    puts("Could not get board ID.\n");
    #endif

    /* Check if baseboard eeprom is available */
    if (i2c_probe(CONFIG_SYS_I2C_EEPROM_ADDR)) {
    puts("Could not probe the EEPROM; something fundamentally "
    "wrong on the I2C bus.\n");
    }

    /* read the eeprom using i2c */
    if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 2, (uchar *)&header,
    sizeof(header))) {
    puts("Could not read the EEPROM; something fundamentally"
    " wrong on the I2C bus.\n");
    }
    #endif

    header.magic = 0xEE3355AA;
    strcpy(header.name, "A335X_SK");//strcpy(header.name, "A335BNLT");
    strcpy(header.version, "1.2B");//strcpy(header.version, "00A6");
    strcpy(header.serial, "45124P196447");//strcpy(header.serial, "4313BBBK1325");
    strcpy(header.config, "SKU#00");


    if (header.magic != 0xEE3355AA) {
    /*
    * read the eeprom using i2c again,
    * but use only a 1 byte address
    */
    if (i2c_read(CONFIG_SYS_I2C_EEPROM_ADDR, 0, 1,
    (uchar *)&header, sizeof(header))) {
    puts("Could not read the EEPROM; something "
    "fundamentally wrong on the I2C bus.\n");
    hang();
    }

    if (header.magic != 0xEE3355AA) {
    printf("Incorrect magic number (0x%x) in EEPROM\n",
    header.magic);
    hang();
    }
    }

    ...

  • 直接把读取E2prom的部分注释掉就可以了,去掉依赖关系