通过学习理解合众达的EVM评估板上的VPIF接口,知道了VPIF是支持标准的BT.1120接口的格式数据。有哪位大神可以告知从TVP7002输出的到底是啥样的标准的数据。因为我们FPGA打算仿照VPIF前端,也就是TVP7002这个功能模块来编写这个接口。但是问题是现在不知道从TVP7002这个位置出来的数据到底是啥样的。它是不是满足标准的BT1120标准。或者说是它的关键位置就是那个EAV和SAV那四个字节怎么配置。还有对于`080P和720P的数据格式的视频数据,在这个BT1120接口标准配置下有什么不一样的(EAV和SAV)