This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP 2407a 烧写问题



2407A 5100 仿真器 烧写时出现如下错误:Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x1d8: Error 0x00000008/-1076 Error during: Break Point,  Cannot set/verify breakpoint at 0x000001D8   Sequence ID: 7 Error Code: -1076 Error Class: 0x00000008

怎么办?

  • 2407是C2000芯片。这个报错是说没有办法设置断点。

    楼主做下面几件事,再试试。

    1、在CCS-->debug-->breakpoints中点remove all。去除所有的breakpoint

    2、在CCSv3-->option-->Cuctomize-->program/project/CIO中的ProgramLoad 中的1,3,4,5打钩

    3、重新编译你的工程,重新烧写FLASH。

    CCSV3.3最新版本下载:

    www.deyisupport.com/.../4292.aspx