This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问DSP/BIOS 程序烧写跟非DSP/BIOS烧写有什么区别???



哪个大神知道?

waring:section flash.out(.text) at 0600008h falls in unconfigured memory (skipped)

.

.

.

好多这样的警告;

hex6x makefile.cmd

flash.out
-a
-order L
-memwidth  8
-image
-map memory.map
ROMS
{
    FLASH: org = 0xB0000000, len = 0x40000, romwidth = 8, files = {image.hex}
}

/****************************************************************************************/

link.cmd

MEMORY
{
    VEC:          o = 0x00800000        l = 0x200
    BOOTRAM:    o = 0x00800200      l = 0x200
//    L2_PRAM:    o = 0x00800400        l = 0xFFC00
//    L2_BRAM:       o = 0x00900000        l = 0x100000
    boot:        o = 0xB0000000       l = 0x400
    FLASH:        o = 0xB0000400          l = 0x3FFD00
//    DDR2:       o = 0xE0000000      l = 0x10000000
}

SECTIONS
{
     "bootload"  >         boot  run =BOOTRAM
    .text       >         FLASH    run = IRAM, LOAD_START(FLASH_TEXT_START), RUN_START(RAM_TEXT_START), SIZE(TEXT_SIZE)
    .cinit      >         FLASH    run = IRAM, LOAD_START(FLASH_CINIT_START), RUN_START(RAM_CINIT_START), SIZE(CINIT_SIZE)
     .const      >        FLASH    run = IRAM, LOAD_START(FLASH_CONST_START), RUN_START(RAM_CONST_START), SIZE(CONST_SIZE)
    .switch     >        FLASH    run = IRAM, LOAD_START(FLASH_SWITCH_START), RUN_START(RAM_SWITCH_START), SIZE(SWITCH_SIZE)
    .data        >        IRAM
    .stack      >       IRAM
    .bss        >       IRAM
    .far        >       IRAM
    .sysmem     >       IRAM
    .cio        >       IRAM
    .vecs        >        FLASH     run = VEC, LOAD_START(FLASH_VECTOR_START), RUN_START(RAM_VECTOR_START), SIZE(VECTOR_SIZE)
}

/***********************************************************************************************************************************************************/

还有DSP/BIOS的.cmd

然后就warning了