This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 EDMA



 您好!

     请问1. 6678里究竟有多少个物理上的DMA通道?是144个吗?

            2.这些DMA通道和TC具有怎样的对应关系?

            3.最多允许几个DMA通道并发传输数据?

      谢谢。

  • 参看6678 data manual EDMA一小节,其中有对6678所拥有的EDMA做详细描述。

    简单来说6678有3个EDMA控制器,其中控制器0有16个EDMA channel,其他两个各有64个EDMA channel,并且每个控制器各有8个QDMA channel。

    每个控制器有多个传输控制器,如控制器0有2个TC,其他两个控制器各有4个TC,每个TC可以并行执行,也就是说做多可能有10个通道在并行执行数据传输。

  • 如果八个核同时传输数据,是否就要使用八个传输控制器,像vlfft中的dma,是否是使用了八个?