This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO传输数据问题



板卡是自己设计的,上面有4块C6678和一块FPGA,

现图像数据摄像头->SAA7115->FPGA->DSP1->DSP4, 如果单独跑DSP1的程序,可以正常接收数据,但是如果开始跑DSP4的程序(只是接收),会发现DSP1和DSP4都无法继续接收数据,先跑DSP4的程序也是一样。

请问下大家这个问题可能是什么导致的呢?谢谢

  • Fan,

                 希望能提供更多的信息,例如DSP1和FPAG以及DSP1和DSP4之间都用了哪些SRIO端口,出现错误的时候,SRIO端口状态是什么?SRIO 数据传输采用的是哪种类型? 有没有试过loopback模式是否可以正常运行?