如题 自己画了一块6678的板子 电源设计等基本参考 6678EVM 只不过 CVDD与VCC1.0 使用了LM21215A + LM10011组合
现在在进行DEBUG调试的时候,总是经常报如下错误,导致JTAG与6678失去连接,但是6678程序依旧在跑(GPIO输出的LED依旧闪烁)
C66xx_0: Power Failure on Target CPU
C66xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
还有,我的DDR目前最高只能跑到967MHz ,但是十分不稳定,最高一次也突然跑到过1333MHz 这样是不是说明我的布线没有问题呢?
目前感觉可能出问题的就是电源纹波太大了,目前CVDD和1.0还有1.5的电源纹波都在150mv到200mv之间(运行状态下),这样是不是纹波太大了呢?
纹波太大导致上述错误呢?但是纹波大,程序为什么不会停呢?
不知道这是为什么,有没有专家帮忙解决一下?
感激不尽啊!