首先要感谢提供www.deyisupport.com/.../4773.aspx
例程的网友!
在调试过程中,不太理解srio_serdes_loopback与SRIO_INTERNAL_LOOPBACK的区别;
还有就是SRIO_EXTERNAL_LOOPBACK与SRIO_EXTERNAL_FORWARD_BACK模式的区别!恳请专家拨云见雾! 不胜感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先要感谢提供www.deyisupport.com/.../4773.aspx
例程的网友!
在调试过程中,不太理解srio_serdes_loopback与SRIO_INTERNAL_LOOPBACK的区别;
还有就是SRIO_EXTERNAL_LOOPBACK与SRIO_EXTERNAL_FORWARD_BACK模式的区别!恳请专家拨云见雾! 不胜感谢!
SERDES_LOOPBACK和EXTERNAL_LOOPBACK需要在两块TCI6670的单板上运行的,如果是单片C6678,建议使用DIGITAL_LOOPBACK.
请问如果我的硬件是采用两片或多片C6678互连, 那么这个例子中实用2个DSP通信的例程是否就可以呢?
当只有一块C6678开发板,无法调试SRIO的互联通信! 环境具备的话,这个例子我认为可以使用,不知理解的对否!
如果有两块6678,那么需要将该程序根据硬件连接进行修改,应该是可以跑通的。另外SERDES_loopback在某些单板上是可以跑通的,你可以参考勘误表中的内容。