This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求解 6678 L2做cache 和 .text 放ddr3 的问题



hi all,

求问两个问题;

1  如果用 cache_setL2size(cache_256kcache),设置,意思是L2(总512k)中256k作为cache使用了,剩余256k作为sram了?那么具体来说哪256k是cache,哪256k是sram呢???在cmd文件中需要注意区分吗???

2 如过用#pragma code_section 吧部分不常用的函数放到ddr3中,对ddr3需要额外配置吗???以前配置用来放数据的ddr3可以直接放程序吗??或者说放程序的ddr3和放数据的ddr3配置完全一致吗???

求解答,万谢!!!