This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 DUMP BAYER数据的问题



使用camra口输入视频,

前端为FPGA产生的1920*1080的BAYER数据,配置ISIF模块的SPH,LNH,SLVx,LNV和CADU,CADL,并启动DWEN写入DDR,从DDR对应位置DUMP出数据完全OK;

把FPGA输出修改为3648*2736 BAYER数据,重新配置了LNH,LNV,此时dump出的数据前2732行均正确,最后四行的数据为8080,

用mem_rdwr.out手动修改最后四行数据为0,再次启动DWEN写数据到DDR,发现最后四行数据仍为0,说明ISIF模块没有向最后四行写数据.

请帮忙分析下原因,另外8127 ISIF模块对输入数据大小有哪些限制?