This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 EVM板子如何使用RDK包



您好:

        最近在使用DM368  EVM板子,想用IPNC的RDK包?用的是IPNC_RDK_DM36x_Version5.1.0开发包(用IPNC_RDK_DM36x_Version4.1.0开发包,结果一样),配置如下:SYSTEM := EVM ;IPNC_PLATFORM := DM368 ; FILESYS_MODE := NFS ;IMGS_ID := IMGS_TVP514X ;编译都通过了。用TFTP形式启动Linux内核,用NFS形式挂载文件系统,系统已经成功启动了,但是

执行av_server( ./av_server.out DM368 AUDIO 8000 AAC 32000 D1 AEWB TI2A H264)时报段错误:Segmentation fault 。

执行./moduletest.out   csl  什么都不显示,直接退出到命令行 ;

执行 ./moduletest.out osa_cmem       系统就死掉了, 报错如下:
   请TI技术支持和各位高手帮助看一下问题所在 ,再次深表谢意!!

 USAGE : ./moduletest.out cmem <size>
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = c0004000
[00000000] *pgd=00000000
Internal error: Oops: 17 [#1] PREEMPT
last sysfs file:
Modules linked in:
CPU: 0    Not tainted  (2.6.37_IPNC_DM365EVM_5.1.0 #1)
PC is at release+0xe4/0x238
LR is at walk_stackframe+0x28/0x44
pc : [<c01eb1bc>]    lr : [<c0031218>]    psr: 00000013
sp : c3313e60  ip : c3313da8  fp : c3313eb4
r10: c04c909c  r9 : 00000004  r8 : 00000000
r7 : 00000001  r6 : 00000000  r5 : c32e2080  r4 : 00000000
r3 : 00000000  r2 : c04c9094  r1 : c04c909c  r0 : 00000000
Flags: nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
Control: 0005317f  Table: 83320000  DAC: 00000015
Process moduletest.out (pid: 1043, stack limit = 0xc3312270)
Stack: (0xc3313e60 to 0xc3314000)
3e60: c3313e84 c048d94c 00000e00 00000000 c32e2080 c04c9094 c04c909c 00000000
3e80: 00000001 00000000 00000000 c32e2088 c32e2080 00000008 00000000 c2c38998
3ea0: c2c35800 c3006820 c3313eec c3313eb8 c00a8a68 c01eb0e8 00000000 00000000
3ec0: c31b75cc c32e2080 00000000 c32cd0c0 0000000c c32cd0c8 c3312000 00000000
3ee0: c3313f0c c3313ef0 c00a5a4c c00a8964 c30fb200 00000001 c32cd0c0 00000000
3f00: c3313f34 c3313f10 c00452f0 c00a59e0 c30fb200 c32cd0c0 c30fb200 000000f8
3f20: c002e1a4 00000000 c3313f4c c3313f38 c00453a0 c0045274 00000000 c3312000
3f40: c3313f74 c3313f50 c0046be8 c004535c 00000000 00000001 00000026 40113000
3f60: c3313fa4 c3313f70 c3313f94 c3313f78 c0047168 c0046a34 00000022 00094f48
3f80: 00094f24 402f5774 c3313fa4 c3313f98 c00471b4 c00470bc 00000000 c3313fa8
3fa0: c002e020 c00471ac 00094f48 00094f24 00000000 00000000 fbad2088 00000008
3fc0: 00094f48 00094f24 402f5774 000000f8 00000000 00000000 4011b000 00000000
3fe0: 40113000 be926cd8 401ff364 40262210 60000010 00000000 835fe031 835fe431
Backtrace:
[<c01eb0d8>] (release+0x0/0x238) from [<c00a8a68>] (fput+0x114/0x1f8)
[<c00a8954>] (fput+0x0/0x1f8) from [<c00a5a4c>] (filp_close+0x7c/0x88)
[<c00a59d0>] (filp_close+0x0/0x88) from [<c00452f0>] (put_files_struct+0x8c/0xe8)
 r6:00000000 r5:c32cd0c0 r4:00000001
[<c0045264>] (put_files_struct+0x0/0xe8) from [<c00453a0>] (exit_files+0x54/0x58)
[<c004534c>] (exit_files+0x0/0x58) from [<c0046be8>] (do_exit+0x1c4/0x688)
 r5:c3312000 r4:00000000
[<c0046a24>] (do_exit+0x0/0x688) from [<c0047168>] (do_group_exit+0xbc/0xf0)
[<c00470ac>] (do_group_exit+0x0/0xf0) from [<c00471b4>] (sys_exit_group+0x18/0x24)
 r6:402f5774 r5:00094f24 r4:00094f48
[<c004719c>] (sys_exit_group+0x0/0x24) from [<c002e020>] (ret_fast_syscall+0x0/0x2c)
Code: e59a4000 e50b3048 ea00003c e1a06004 (e4961008)
---[ end trace 34c2a3dc0288df80 ]---
Fixing recursive fault but reboot is needed!