This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678的ibl镜像i2crom_0x51_c6678_le.bin, 前32个byte就是所谓的boot parameter table吗?



c6678的ibl镜像i2crom_0x51_c6678_le.bin这个文件满足文件档里说的

boot  parameter table

-------------------------------

entry point: __c_int00

---------------------------------

boot table

---------------------------

这种结构吗?