This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP6713 内存分配问题



工程师您好!我想将Sun_Emif_Init()这个函数加载到CE3_SDRAM,然后在IRAM里运行,写了下面的两段程序,可为什么一运行就到Sun_Emif_Init()函数的第一行停了?想实现这个应该怎么写?
---------------------------------------------------------------------------------------------
SECTIONS
{    
        Emif_Init: {}          load > CE3_SDRAM,
                                        run > IRAM,
                                        RUN_START(_Emif_Init_runstart),
                                        LOAD_START(_Emif_Init_loadstart),
                                        LOAD_END(_Emif_Init_loadend)
    .text:    {} > IRAM
    .switch:  {} > IRAM
    .cinit:   {} > IRAM
    .pinit:   {} > IRAM
    .const:   {} > IRAM
    .stack                 > IRAM
    .sysmem                 > IRAM
    .csldata         > IRAM
    .bss:     {} > IRAM 
    .far:     {} > IRAM
    .data:    {} > IRAM
    .cio:     {} > IRAM
}
-----------------------------------------------------------------------------------------------------
extern unsigned int Emif_Init_runstart;
extern unsigned int Emif_Init_loadstart;
extern unsigned int Emif_Init_loadend;

#pragma CODE_SECTION(Sun_Emif_Init,"Emif_Init")
void Sun_Emif_Init()
{
        //两种初始方式,一种如MyEMIFcfg0用宏语言,一种如MyEMIFcfg1直接赋值

        EMIF_Config MyEMIFcfg1 = {
    0x00003068,        /*  Global Control Reg. (GBLCTL)   */
    0x22920712,        /*  CE0 Space Control Reg. (CECTL0)    setup 2, Wstrobe 10, Rstrobe 7,hold 2 */
    0x513a8502,        /*  CE1 Space Control Reg. (CECTL1)   */
    0x10510191,        /*  CE2 Space Control Reg. (CECTL2)   */
    0x10510191,        /*  CE3 Space Control Reg. (CECTL3)   */
    0x6b227000,        /*  SDRAM Control Reg.(SDCTL)   */
    0x00000300,        /*  SDRAM Timing Reg.(SDTIM)   */
    0x00000128         /*  SDRAM Extended Reg.(SDEXT)   */
    };
        EMIF_config(&MyEMIFcfg1);
}

-------------------------------------------------------------------------------------------------------------