This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工程师好!
我们使用了Appro IPNC dm368的解决方案,目前项目需要连接usb外设,所以要求将usb模式从device模式更改为host模式。
之前已经按照ti工程师的建议修改了相应的内核配置,可以在 demsg | grep usb 命令下看到下列结果:
[ 0.145455] usbcore: registered new interface driver usbfs
[ 0.146965] usbcore: registered new interface driver hub
[ 0.147913] usbcore: registered new device driver usb
[ 0.245086] musb-hdrc: version 6.0, host, debug=0
[ 0.245289] musb-hdrc musb-hdrc: dma type: dma-cppi3
[ 0.260721] musb-hdrc: ConfigData=0x06 (UTMI-8, dyn FIFOs, SoftConn)
[ 0.260777] musb-hdrc: MHDRC RTL version 1.500
[ 0.260807] musb-hdrc: setup fifo_mode 2
[ 0.260851] musb-hdrc: 9/9 max ep, 4032/4096 memory
[ 0.260944] musb-hdrc musb-hdrc: MUSB HDRC host driver
[ 0.261188] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1
[ 0.284651] musb-hdrc musb-hdrc: USB Host mode controller at fec64000 using DMA, IRQ 12
[ 0.435430] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
[ 2.602524] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
[ 4.752588] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
[ 6.902624] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
应该可以确认内核已经设置为host模式了,但是无法识别usb设备(U盘和USB wifi),同时出现了 VBUS error workaround (delay coming) ,并且我们
从外部电源直接供电5v给VBUS仍然会出现这个错误,所以现在想请教高手两个问题:
1.出现“VBUS error workaround (delay coming)”的错误信息一般是出于什么原因?
2. appro ipnc dm368要从device模式更改为host模式,除了内核方面的修改外,还需要在硬件上边做什么修改吗?
(目前我们只注意到USB_VBUS和USB_ID)
希望可以得到高手的帮助,万分感谢!!!
您好,
请问你的问题解决了吗?我遇到你同样的问题;
# modprobe davinci.ko
[ 67.432507] musb-hdrc: version 6.0, host, debug=0
[ 67.611615] musb-hdrc musb-hdrc: dma type: pio
[ 67.651516] musb-hdrc: ConfigData=0x06 (UTMI-8, dyn FIFOs, SoftConn)
[ 67.663010] musb-hdrc: MHDRC RTL version 1.500
[ 67.671115] musb-hdrc: setup fifo_mode 2
[ 67.696872] musb-hdrc: 9/9 max ep, 4032/4096 memory
[ 67.720536] musb-hdrc musb-hdrc: MUSB HDRC host driver
[ 67.731249] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1
[ 67.783931] hub 1-0:1.0: USB hub found
[ 67.789600] hub 1-0:1.0: 1 port detected
[ 67.832160] musb-hdrc musb-hdrc: USB Host mode controller at fec64000 using PIO, IRQ 12
[ 67.949099] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
dfsafsd sam 说:hi Chris,
你好关于DM368 EVM 能否同时支持USB HOST 和 usb Peripheral (gadget stack) 这两种模式啊
你好,
什么叫同时支持?控制器同一个时刻只可能是一种模式。
你好,
你需要配置USB驱动为OTG,网上已有客户实现:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/7651/30350
rebuilt the kernel and modules, and installed the new modules.
Now the USB OTG is working well on the DM365 EVM board (with LSP 2.10) when I use the NFS file system.
但请注意,你插入的设备必须支持/有USB ID引脚,因为驱动是通过这个引脚的信号来判断插入的设备是host还是device。
Hi Chris,
将内核配置成OTG 出现如下问题:
[ 48.670937] musb-hdrc: version 6.0, otg (peripheral+host), debug=0
[ 48.783382] musb-hdrc musb-hdrc: dma type: dma-cppi3
[ 48.808040] musb-hdrc: ConfigData=0x06 (UTMI-8, dyn FIFOs, SoftConn)
[ 48.814559] musb-hdrc: MHDRC RTL version 1.500
[ 48.821359] musb-hdrc: setup fifo_mode 2
[ 48.825396] musb-hdrc: 9/9 max ep, 4032/4096 memory
[ 48.833324] musb-hdrc musb-hdrc: USB OTG mode controller at fec64000 using DMA, IRQ 12
[ 48.980247] g_file_storage gadget: No serial-number string provided!
[ 48.989641] g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
[ 48.999403] g_file_storage gadget: Number of LUNs=1
[ 49.004419] g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/mmcblk0
[ 49.013932] musb-hdrc musb-hdrc: MUSB HDRC host driver
[ 49.020944] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1
[ 49.052174] hub 1-0:1.0: USB hub found
[ 49.056122] hub 1-0:1.0: 1 port detected
[ 49.215042] davinci_musb_interrupt 351: VBUS error workaround (delay coming)
你好,
如果上电就插u盘可以识别么?
你有按照下面的链接来配置和使用么?
https://developer.ridgerun.com/wiki/index.php/How_to_configure_DM365_for_USB_host,_device_and_OTG_support#USB_On-The-Go_.28OTG.29_functionality
DM368 USB不支持在USB线连上后再次动态切换模式。
hi Chris,
DM368能读到USB 信息,但是找不到USB 设备:
# modprobe davinci.ko
[ 170.367384] musb-hdrc musb-hdrc: dma type: dma-cppi3
[ 170.412098] DaVinci OTG revision 00140901 phy 21f0 control 00
[ 170.422745] musb-hdrc: ConfigData=0x06 (UTMI-8, dyn FIFOs, SoftConn)
[ 170.445525] musb-hdrc: MHDRC RTL version 1.500
[ 170.453795] musb-hdrc: setup fifo_mode 2
[ 170.473847] musb-hdrc: 9/9 max ep, 4032/4096 memory
[ 170.482401] musb-hdrc musb-hdrc: MUSB HDRC host driver
[ 170.513496] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1
[ 170.560620] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 170.571234] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 170.595018] usb usb1: Product: MUSB HDRC host driver
[ 170.603568] usb usb1: Manufacturer: Linux 2.6.37_IPNC_DM368_5.1.0+ musb-hcd
[ 170.631888] usb usb1: SerialNumber: musb-hdrc
[ 170.661929] hub 1-0:1.0: USB hub found
[ 170.682070] hub 1-0:1.0: 1 port detected
[ 170.693172] musb-hdrc musb-hdrc: USB Host mode controller at fec64000 using DMA, IRQ 12
[ 170.720144] Registered /proc/driver/musb_hdrc
[ 171.151733] usb 1-1: new high speed USB device using musb-hdrc and address 2
[ 171.329569] usb 1-1: New USB device found, idVendor=0930, idProduct=6545
[ 171.340041] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 171.370974] usb 1-1: Product: DT 101 G2
[ 171.390661] usb 1-1: Manufacturer: Kingston
[ 171.397437] usb 1-1: SerialNumber: 1301091703A3
问题解决,内核配置问题:
Device Drivers ---> SCSI device support ---> <*> SCSI device support [*] legacy /proc/scsi/support --- SCSI support type (disk, tape, CD-ROM) <*> SCSI disk support USB support ---> <*> Support for Host-side USB *** Miscellaneous USB options *** [*] USB device filesystem [*] USB device class-devices (DEPRECATED) *** USB Host Controller Drivers *** <*> Inventra Highspeed Dual Role Controller (TI, ...) *** OMAP 343x high speed USB support *** Driver Mode (USB Host) ---> [ ] Disable DMA (always use PIO) [*] Use System DMA for Rx endpoints [*] Enable debugging messages --- USB Device Class drivers <*> USB Mass Storage support
哥们 ,我也遇到和你一样的问题, 但是我根据你上面的 make menuconfig 配置,看了一下我得,和你就差 Enable debugging messages 这个选项 没选其他都一样的,这个问题,难道只是这个配置问题造成的吗?